This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x Wince7 显示驱动发生 ‘Data Abort‘ 无法正常启动



你好:

   我的BSP是Wince7 AM33x_BSP, 编译烧写完成之后启动在 am33x_display 发生 ‘Data Abort’。

1. 我的启动信息如下:

Load NK image from flash memory
IsValidMBR: MBR sector = 0x480 (valid MBR)
OpenPartition: Partition Exists=0x1 for part 0x20.
BP_SetDataPointer at 0x0

ROMHDR (pTOC = 0x83c98fa0) ---------------------
DLL First : 0x4001eefa
DLL Last : 0x436df000
Physical First : 0x80002000
Physical Last : 0x83c9cf50
Num Modules : 373
RAM Start : 0x83ca0000
RAM Free : 0x83cb5000
RAM End : 0x8a800000
Num Copy Entries : 2
Copy Entries Offset : 0x8123af44
Prof Symbol Length : 0x00000000
Prof Symbol Offset : 0x00000000
Num Files : 153
Kernel Flags : 0x00000000
FileSys RAM Percent : 0x0a0a0a0a
Driver Glob Start : 0x00000000
Driver Glob Length : 0x00000000
CPU : 0x01c2
MiscFlags : 0x0002
Extensions : 0x80003020
Tracking Mem Start : 0x00000000
Tracking Mem Length : 0x00000000
------------------------------------------------

NK Image Loaded
Launch Windows CE image by jumping to 0x80002000...

Windows CE Kernel for ARM (Thumb Enabled)
CPU CP15 Control Register = 0xc5387f
CPU CP15 Auxiliary Control Register = 0x42
Board Name: EZ335X
Board Ver : 1.0A
+OALTimerInit(1, 24000, 200)
--- High Performance Frequecy is 24 MHz---
PID:00400002 TID:00410002 SetOpp to 3 
PID:00400002 TID:01320006 ECC TYPE is BCH 8 bit with ELM
PID:00400002 TID:01320006 8Bit NAND device
PID:00400002 TID:01320006 CM3: input file [\windows\firmware.bin] is 9932 bytes long
PID:00400002 TID:01320006 CM3: firmware file read ok!
PID:00400002 TID:01320006 Cpsw3g_InitializeAdapter: mode=1, port=1, txCh=0, rxChMask=0x01, ActiveCpgmac=1
PID:00400002 TID:01320006 SDHC: CPU revision 0xffffffff
PID:00400002 TID:01320006 SDHC host controller initialize: m_fastPathSDIO:1 m_fastPathSDMEM:0
PID:00400002 TID:01320006 CAM3xxOTG::Init DEVCTL 80
PID:00400002 TID:01320006 CAM3xxOTG::Init DEVCTL 80
PID:00400002 TID:05980002 Exception 'Data Abort' (0x4): Thread-Id=05980002(pth=9e46b7d0), Proc-Id=00400002(pprc=83cae5e0) 'NK.EXE', VM-active=00400002(pprc=83cae5e0) 'NK.EXE'
PID:00400002 TID:05980002 PC=ef0ccf80(am33x_display.dll+0x0001cf80) RA=00000000(???+0x00000000) SP=aec0f434, BVA=00000000
PID:00400002 TID:05980002 Exception 'Data Abort' (0x4): Thread-Id=05980002(pth=9e46b7d0), Proc-Id=00400002(pprc=83cae5e0) 'NK.EXE', VM-active=00400002(pprc=83cae5e0) 'NK.EXE'
PID:00400002 TID:05980002 PC=efdd2aa0(gwes.dll+0x00062aa0) RA=00000090(???+0x00000090) SP=aec0fdc0, BVA=0000010c

2.我的display注册表如下:

;===============================================================================
; AM335x Display driver (LCDC)
; @CESYSGEN IF CE_MODULES_DISPLAY
; --> Entering C:\WINCE700\platform\AM33X_BSP\src\drivers\display\display.reg
; All rights reserved ADENEO EMBEDDED 2010
;===============================================================================
; @CESYSGEN IF CE_MODULES_DISPLAY

[HKEY_LOCAL_MACHINE\SYSTEM\GWE]
; "PORepaint"=dword:0 - the display driver handles everything
; "PORepaint"=dword:1 - gwe should save and restore the bits
; "PORepaint"=dword:2 - gwe should invalidate and repaint
; "PORepaint"=dword:3 - gwe and driver need to save video memory
;
"PORepaint"=dword:0

[HKEY_LOCAL_MACHINE\System\GDI\Drivers]
"IRQ"=dword:24
"Display"="am33x_display"
; 0 for flat surface manager, 1 for VRFB surface manager
; Note only flat surface manager is supported
"SurfaceMgr" = dword:0

; sets initial screen rotation
; use 0 for 0 degree, 1 for 90 degree, 2 for 180 degree and 4 for 270 degree
; Note: Rotation should not be used with the flat frame buffer, memory/bus bandwidth may
; be exceeded by display scanning requirements causing display to flicker and/or lock up.
"Angle" = dword:0
"PowerFlags"=dword:00000103 ; send pre/post device state changes
"membase"=multi_sz:"48050000","48306B00"
"memlen"=multi_sz:"00000100","00000100"
; controls software based mouse cursor emulation, 0 = disable, 1 = enable
; Note that OS configuration must include mouse cursor support (sysgen_cursor).
; Note that display performance will be reduced when cursor support is enabled.
; Note that cursor support has not been tested with direct draw, overlays or rotation.
; @CESYSGEN IF GWES_MCURSOR
"Cursor"=dword:1
; @CESYSGEN ENDIF GWES_MCURSOR
; Set to 1 to enable wait for vertical blank support
"EnableWaitForVerticalBlank"=dword:1
"EnableNeonBlts"=dword:1
"EnableDMABlts"=dword:1
"EnableOverlay"=dword:0 
"HardwareRotation"=dword:0 
"DMAFill"=dword:0

; Revert logic in common.reg that turns display off during SystemIdle.
; PMCLASS_DISPLAY_GUID
[HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Control\Power\State\SystemIdle\{EB91C7C9-8BF6-4a2d-9AB8-69724EED97D1}]
"Default"=dword:2 ; D2

; Not supported
;[HKEY_LOCAL_MACHINE\System\GDI\ROTATION]
; ; rotates screen - use 0 for 0 degree 5a for 90 degree, b4 for 180 degree and 10e for 270 degree
; "Angle"=dword:0

[HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\MediaPlayer\Preferences]
"RenderMethod"=dword:2

[HKEY_LOCAL_MACHINE\Software\Microsoft\DirectX\DirectShow\VMR]
"RenderingPrefs"=dword:8

; Bits per pixel setting for compositor backbuffers
[HKEY_LOCAL_MACHINE\SYSTEM\GWE\Compositor]
"OpaqueBufferBPP"=dword:10

; @CESYSGEN ENDIF CE_MODULES_DISPLAY
; <-- Leaving C:\WINCE700\platform\AM33X_BSP\src\drivers\display\display.reg
; @CESYSGEN ENDIF CE_MODULES_DISPLAY

3.定位bug位置   RVA+base = 0x0001cf80 - 0x1000 = 0x1bf80

查看am33x_display.map 文件

0001:0001ad28 ?PhysicalAddr@OMAPVrfbSurface@@UAAKW4OMAP_DSS_ROTATION@@HW4OMAP_ASSOC_SURF_USAGE@@@Z 1001bd28 f omap_ddgpe_lcdcai:surfmgr_vrfb.obj
0001:0001af84 ?PixelIncr@OMAPVrfbSurface@@UAAKW4OMAP_DSS_ROTATION@@H@Z 1001bf84 f omap_ddgpe_lcdcai:surfmgr_vrfb.obj

这里我有疑问 我注册表里的SurfaceMgr=0,应该使用OMAPFlatSurface这个类,为什么会调用OMAPVrfbSurface类里的函数?

另外是不是我的BSP配置选项有问题,组件问题导致了启动问题?

这个BUG的可能原因?

hainan

  • 请问您是在我们的TI的GPEVM板子上测试的吗?

  • 我是在定制版上,大部分功能没有修改。

    问题可能出在wince注册表、组件选择上

  • 我们的WinCE包在demo板上的dsiplay功能是没问题的,你如果换了个屏,应该只需要把timming重新调整一下就可以了,应该不需要改太多的东西

  • 你好:

    通过跟踪源码发现:

    1. Omap_ddgpe.cpp中OMAPDDGPE::OMAPDDGPE() 

       if( m_pDisplayContr->InitLCD() == FALSE )初始化失败, 继续跟踪

    2.Lcdcai.cpp中OMAPDisplayController::InitLCD()

        lcdc_set_update_mode(&m_lcdc, FB_AUTO_UPDATE);更新模式出错,继续跟踪发现

    3.Lcdc.c 中int lcdc_set_update_mode(struct lcdc* lcdc,enum fb_update_mode mode)

      lcdc_load_palette(lcdc);载入调色板出错

      这里 fb_update_mode mode 有两种模式FB_AUTO_UPDATE 和FB_UPDATE_DISABLED,前者会需要调色相关配置,继续跟踪

    4.Lcdc.c中static void lcdc_load_palette(struct lcdc* lcdc)

      palette = (UINT16 *)lcdc->palette_virt;

     *(UINT16 *)palette &= 0x0fff;

      这里对调色板虚拟地址进行赋值, 在我的BSP中没有对调色板分配内存,所以发生 'Data Aboart' 错误。

     

     因而我使用FB_UPDATE_DISABLED模式,我的显示屏是RGB16,不知道选择该模式会有什么影响?

     调色板具体如何分配和使用?