大神们:
你们谁有使用过AM3352 是使用的1.8V的NANDFLASH呀,我的有点问题,启动加载不了MLO文件。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
一般3.3V用的比较多,你现在遇到的NAND读写问题,是仅仅在启动时出现,还说到UBoot,kernel时一样存在?
建议你,首先确认一下,当前的NAND启动时序是可以被支持的,参考TRM的26.1.7.4 NAND章节;再者,可以确认一下NAND本身的硬件设计是没问题的,比如用SD卡启动后,在UBOOT中对NAND进行读写看是否正常。
请问你对应连接NAND的GPMC AD0-AD7给的供电SHV1也是1.8V么?
有没有用示波器抓过数据线上的data?