all:
我目前想在dm385上移植一些自己的算法,比如说检测越界算法等等!有下面几个问题需要咨询一下:
1. dm385上面跑算法,能不能在LOW_POWER模式下实现,我发现FULL_FEATURE模式下编译出来的程序在dm385上面跑不起来。
2. 有没有文档讲在M3VPSS上面移植算法,或者麻烦各位简述一下流程。
由于项目时间问题,希望有人能帮我尽快回复,我将感激不尽!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
1. low power主要是关闭了HDVPSS和vpss M3上的协处理器。请问你的算法运行在哪里?A8还是m3?
2.vpss M3上已经在运行了2A算法了,请确保m3的cpu性能对你的算法足够。你能否在A8上运行你的算法呢?