TI专家,各位朋友:
OMAPL138 CPU工作在300M的时候,我看很多情况下EMIFA的时钟配置的都是100M,现在CPU工作在456M的频率下,EMIFA时钟最高能配置在多少?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不管是300MHz还是456MHz, EMIFA时钟最高频率都是100MHz, 可以看下面的表里ASYNC1参数。
Table 6-5. Maximum Internal Clock Frequencies at Each Voltage Operating Point
http://www.ti.com/lit/ds/symlink/omap-l138.pdf
有新的问题,麻烦另起新帖。
a) EMAC module是由PLL0_SYSCLK4给的。
b) PLL0_SYSCLK7可以作为RMII模式下的时钟源。MII模式必须用外部时钟源。
c) 不建议用PLL0_SYSCLK7作为时钟源,下面的文档上有这样的note.
NOTE:
The SYSCLK7 output clock does not meet the RMII reference clock specification of 50 MHz +/-50 ppm.
http://www.ti.com/lit/ug/spruh77a/spruh77a.pdf