DM8148EVM 板子
这里是720P输出,timing的时钟理论应当是74250,被我修改为148500;用示波器测量发现输出还是74250;(vpshal_hdvenc.c中修改的)
请问我应当怎么样修改时钟输出的实际值?
我现在的问题是480P输出的时钟理论上应当为27MHz,但是出来的是270MHz,想查出怎么控制时钟频率的输出;
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DM8148EVM 板子
这里是720P输出,timing的时钟理论应当是74250,被我修改为148500;用示波器测量发现输出还是74250;(vpshal_hdvenc.c中修改的)
请问我应当怎么样修改时钟输出的实际值?
我现在的问题是480P输出的时钟理论上应当为27MHz,但是出来的是270MHz,想查出怎么控制时钟频率的输出;
Hi VENC最高就是165M应该没有能力输出270MHz的。
你是在EZSDK上面进行修改?
BR,
Eason
在DVRRDK上调试的,
值我没有修改,我是设置为480P模式输出,其他高分辨率都可以正常出画面,但是480P的没有画面,实在找不出问题,测试了输出时钟,结果测试出为270M
DVRRDK 上有demo可以直接切到480p的分配率(NTSC或者VGA)
你可以用Decode+Display DEMO来验证,在display setting->change resolution下面。
我手头暂无支持该分辨率的屏,找到可以帮你一试