This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
按http://processors.wiki.ti.com/index.php/Sitara_Linux_Training:_Hands_on_with_the_SDK,进行了配置,编译执行,RES执行,都ok,但是在GDB配置后进行Debug执行,产生了错误,程序很简单就是helloworld。
如何解决?本人菜鸟,多多帮助,非常感谢!!!
我确认一下,你现在A8核能连接成功吗?
前面CCS对ARM的初始化工作都进行了吗?返回结果也都正常吗?比如CCS的配置,GEL脚本之类的。
可以连接成功,我把ccs编译好的可执行文件,用RES或者拷贝到开发板,是可以执行的,但是就是GDB不行。我在网络上搜了一下,应该是CCS和GDB的版本不匹配,貌似SDK7.0的GDB少了一些什么命令。我用的是CCS5.1.1就是开发板SD卡中的那个版本,SDK用的7.0。请问好用的版本搭配是那种?SDK7.0要用CCS多少才行?http://processors.wiki.ti.com/index.php/Sitara_Linux_Training:_Hands_on_with_the_SDK给的是CCS5.3但是SDK是6.0.
另外QT的配置也出现了问题,按http://processors.wiki.ti.com/index.php/Sitara_Linux_Training:_Hands_on_with_QT配置后,出现了
按照http://processors.wiki.ti.com/index.php/Sitara_Linux_Training:_Hands_on_with_QT上的说明只要配置了工具链后那个就会变成警告而不是错误,我配置了工具链后仍然出现此错误,提示QT没有正确安装。是QTcreator版本问题么?搭配SDK7.0的好用的QTcreator版本是哪种?
真心非常感谢!!!
问题解决了,就是我之前说的CCS与GDB的版本搭配问题,我用的SDK7.0,安装从新安装了CCS5.5(之前用的开发板SD卡中的5.1),后就可以单步调试了。非常感谢大家。