This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: 裸机程序接EMMC卡读写异常

Part Number: AM3352

单板使用 SOC_MMCHS_1_REGS 连接 MTFC8GAKAJCN-4M IT(多媒体卡芯片),驱动参考“AM335X_StarterWare_02_00_01_01” 的hsMmcSdRw工程  更改的。
   程序中收发数据采用的查询方式实现的,目前卡识别功能正常,数据读写功能不正常,辛苦帮忙看下那部分的设置有问题。

unsigned char emmc_wr_test(void)
{
    unsigned char sd_size;
    unsigned char state;
//    unsigned char i=0;

   for(sd_size=0;sd_size<128;sd_size++)
   {
       r_buf[sd_size] = 0;
       w_buf[sd_size] =1+sd_size;
   }
   state =MMCSDWriteCmdSend(&ctrlInfo, w_buf,r_buf, 1,1);
   if(!state)
   {
       return state;
   }

   for(sd_size=0;sd_size<128;sd_size++)
   {
      if(r_buf[sd_size]!=w_buf[sd_size])
      {
           state =0;
           break;
      }
   }

   state = 1;
   return state;

}
   /**
* \brief   This function 实现SD卡的读写测试功能.
*
* \param    mmcsdCtrlInfo It holds the mmcsd control information.
* \param    ptr           It determines the address from where data has to written
* \param    r_ptr         It determines the address from where data has to read
* \param    block         It determines to which block data to be written
* \param    nblks         It determines the number of blocks to be written
*
* \returns  1 - successfull written of data.
*           0 - failure to write the data.
**/
unsigned int MMCSDWriteCmdSend(mmcsdCtrlInfo *ctrl, void *ptr, void *r_ptr, unsigned int block,
                               unsigned int nblks)
{
    mmcsdCardInfo *card = ctrl->card;
    unsigned int status = 0, i=0;
    unsigned int address;
    mmcsdCmd cmd;
    unsigned char state =0;//mmc card state
    /*
     * Address is in blks for high cap cards and in actual bytes
     * for standard capacity cards
     */
    if (card->highCap)
    {
        address = block;
    }
    else//MMC card 和低容量的SD卡一样
    {
        address = block * card->blkLen;
    }

    /* Clean the data cache. */
    CacheDataCleanBuff((unsigned int) ptr, (512 * nblks));

   // ctrl->xferSetup(ctrl, 0, ptr, 512, nblks);
    /*cmd7      */
    cmd.flags = SD_CMDRSP_BUSY;
    cmd.arg = card->rca << 16;
    cmd.nblks = nblks;
    cmd.idx = SD_CMD(7);
    status = MMCSDCmdSend(ctrl, &cmd);

    //数据发送后,SD_RSP10=0x00000700;这里状态是正确的,mmc卡的状态为stby
    if (status == 0)
    {
        return 0;
    }

    state =(cmd.rsp[0]>>9)&0x0F;//state 的值为3,emmc卡的状态变为传送态,后面的指令才有意义
    HWREG(ctrl->memBase + MMCHS_BLK)|=0x200;//set 512 bytes block length

    if(state !=3)//cmd7 指令异常
    {
        return 0;
    }

      /*cmd13   read card states   */
      cmd.flags = SD_CMDRSP_NONE;
      cmd.arg = card->rca << 16;
      cmd.idx = SD_CMD(13);
      status = MMCSDCmdSend(ctrl, &cmd);

      //数据发送后,SD_RSP10=0x00000700;这里状态是错误 的,mmc卡的状态应该为trans,  问题:这里的状态错误怎么改正???
      if (status == 0)
      {
          return 0;
      }
    /*cmd16 设置块的长度*/
    cmd.flags = SD_CMDRSP_NONE;
    cmd.arg = 0x200;
    cmd.idx = SD_CMD(16);
    status = MMCSDCmdSend(ctrl, &cmd);


    if (status == 0)
    {
        return 0;
    }

    state =(cmd.rsp[0]>>9)&0x0F;
    //数据发送后,SD_RSP10=0x00000700;这里状态是错误 的,mmc卡的状态应该为trans,目前为stdby,问题:怎样改???
    /*cmd24 写单个块的值*/
    cmd.flags = SD_CMDRSP_WRITE | SD_CMDRSP_DATA;
    cmd.arg = address;
    cmd.nblks = nblks;

    if (nblks > 1)
    {
        cmd.idx = SD_CMD(25);
        cmd.flags |= SD_CMDRSP_ABORT;
    }
    else
    {
        cmd.idx = SD_CMD(24);
    }


    status = MMCSDCmdSend(ctrl, &cmd);
    //数据发送后,SD_RSP10=0x00000900;这里状态是正确,mmc卡的状态为trans,
    if (status == 0)
    {
        return 0;
    }
//    /*cmd13   read card states   */
//    cmd.flags = SD_CMDRSP_NONE;
//    cmd.arg = card->rca << 16;
//    cmd.idx = SD_CMD(13);
//    status = MMCSDCmdSend(ctrl, &cmd);
//    //数据发送后,SD_RSP10=0x00000900;这里状态是错误 的,mmc卡的状态应该为rcv 问题:怎样改正????,
//    if (status == 0)
//    {
//        return 0;
//    }
    //write data  SD_STAT =0,问题 状态值为何为0???
//    HWREG(ctrl->memBase + MMCHS_BLK)|=0x200;//set 512 bytes block length
    IntMasterIRQDisable();
    while(!((HWREG(ctrl->memBase + MMCHS_STAT) & MMCHS_STAT_TC) >>MMCHS_STAT_TC_SHIFT))
    {
        for (i = 0; i <128; i++)
        {
            if((HWREG(ctrl->memBase + MMCHS_PSTATE) &MMCHS_PSTATE_BWE)>>MMCHS_PSTATE_BWE_SHIFT)
                    HWREG(ctrl->memBase + MMCHS_DATA) = ((unsigned int*)ptr)[i]; //问题:在这里写入时,看不到Data寄存器的数据变化
            else
            {
                break;
            }
        }
//        if(i == 128)
//        {
//            break;
//        }
    }
    IntMasterIRQEnable();
//   status = ctrl->xferStatusGet(ctrl);
    if((HWREG(ctrl->memBase + MMCHS_STAT) & MMCHS_STAT_TC) >>MMCHS_STAT_TC_SHIFT)
    {
        HWREG(ctrl->memBase + MMCHS_STAT) |=1 <<MMCHS_STAT_TC_SHIFT;
    }

    /*cmd17 读取数据*/
       cmd.flags = SD_CMDRSP_READ | SD_CMDRSP_DATA;
       cmd.arg = address;
       cmd.nblks = nblks;

       if (nblks > 1)
       {
           cmd.flags |= SD_CMDRSP_ABORT;
           cmd.idx = SD_CMD(18);
       }
       else
       {
           cmd.idx = SD_CMD(17);
       }

       status = MMCSDCmdSend(ctrl, &cmd);

//       while(!(HWREG(ctrl->memBase + MMCHS_STAT) & MMCHS_STAT_CC));
//
//       HWREG(ctrl->memBase + MMCHS_STAT) |=1 <<MMCHS_STAT_CC_SHIFT;//清楚指令完成标志位

       if (status == 0)
       {
           return 0;
       }

       IntMasterIRQDisable();
       while(!((HWREG(ctrl->memBase + MMCHS_STAT) & MMCHS_STAT_TC) >>MMCHS_STAT_TC_SHIFT))
      {
          for (i = 0; i <128; i++)
          {
              if((HWREG(ctrl->memBase + MMCHS_PSTATE) &MMCHS_PSTATE_BRE)>>MMCHS_PSTATE_BRE_SHIFT)
                  ((unsigned int*)r_ptr)[i]= HWREG(ctrl->memBase + MMCHS_DATA); //问题:这里可以读到值,所有的读取值一样,和写入的值不一样
          }

      }
      IntMasterIRQEnable();

//    if (status == 0)
//    {
//        return 0;
//    }

    /* Send a STOP */
    if (cmd.nblks > 1)
    {
        status = MMCSDStopCmdSend(ctrl);

        if (status == 0)
        {
            return 0;
        }
    }

    return 1;
}

问题1:程序中标注的几个问题,指令发送后,响应的状态位不对?
问题2:关于cache的代码是必须的吗?CacheDataCleanBuff()?