大家好,
************************************************************************************************
我想实现的是多核对外发送 SRIO Doorbell包,遇到了LSU TX error的问题。如下所述
************************************************************************************************
SRIO配置如下:
UInt8 isAllocated;
Srio_DrvConfig drvCfg;
System_printf ("Core Num = %d\n", corenum);
/* Initialize the SRIO Driver Configuration. */
memset ((Void *)&drvCfg, 0, sizeof(Srio_DrvConfig));
/* Initialize the OSAL */
if (Osal_dataBufferInitMemory(SRIO_MAX_MTU) < 0)
{
System_printf ("Error: Unable to initialize the OSAL. \n");
return -1;
}
/********************************************************************************
* The SRIO Driver Instance is going to be created with the following properties:
* - Driver Managed
* - Interrupt Support (Pass the Rx Completion Queue as NULL)
********************************************************************************/
/* Setup the SRIO Driver Managed Configuration. */
drvCfg.bAppManagedConfig = FALSE;
/* Driver Managed: Receive Configuration */
drvCfg.u.drvManagedCfg.bIsRxCfgValid = 1;
drvCfg.u.drvManagedCfg.rxCfg.rxMemRegion = Qmss_MemRegion_MEMORY_REGION1;//Qmss_MemRegion_MEMORY_REGION1;//Qmss_MemRegion_MEMORY_REGION0
drvCfg.u.drvManagedCfg.rxCfg.numRxBuffers = 4;
drvCfg.u.drvManagedCfg.rxCfg.rxMTU = SRIO_MAX_MTU;
/* Accumulator Configuration. */
{
int32_t coreToQueueSelector[4];
/* This is the table which maps the core to a specific receive queue. */
coreToQueueSelector[0] = 736;//736;//704
coreToQueueSelector[1] = 737;
coreToQueueSelector[2] = 738;
coreToQueueSelector[3] = 739;
/* Since we are programming the accumulator we want this queue to be a HIGH PRIORITY Queue */
drvCfg.u.drvManagedCfg.rxCfg.rxCompletionQueue = Qmss_queueOpen (Qmss_QueueType_HIGH_PRIORITY_QUEUE,
coreToQueueSelector[corenum], &isAllocated);
System_printf ("Test Point 4\n");
if (drvCfg.u.drvManagedCfg.rxCfg.rxCompletionQueue < 0)
{
System_printf ("Error: Unable to open the SRIO Receive Completion Queue\n");
return 0;
}
/* Accumulator Configuration is VALID. */
drvCfg.u.drvManagedCfg.rxCfg.bIsAccumlatorCfgValid = 1;
/* Accumulator Configuration. */
drvCfg.u.drvManagedCfg.rxCfg.accCfg.channel = corenum+16;//corenum;//1
drvCfg.u.drvManagedCfg.rxCfg.accCfg.command = Qmss_AccCmd_ENABLE_CHANNEL;
drvCfg.u.drvManagedCfg.rxCfg.accCfg.queueEnMask = 0;
drvCfg.u.drvManagedCfg.rxCfg.accCfg.queMgrIndex = coreToQueueSelector[corenum];
drvCfg.u.drvManagedCfg.rxCfg.accCfg.maxPageEntries = 2;
drvCfg.u.drvManagedCfg.rxCfg.accCfg.timerLoadCount = 0;
drvCfg.u.drvManagedCfg.rxCfg.accCfg.interruptPacingMode = Qmss_AccPacingMode_LAST_INTERRUPT;
drvCfg.u.drvManagedCfg.rxCfg.accCfg.listEntrySize = Qmss_AccEntrySize_REG_D;
drvCfg.u.drvManagedCfg.rxCfg.accCfg.listCountMode = Qmss_AccCountMode_ENTRY_COUNT;
drvCfg.u.drvManagedCfg.rxCfg.accCfg.multiQueueMode = Qmss_AccQueueMode_SINGLE_QUEUE;//Qmss_AccQueueMode_SINGLE_QUEUEQmss_AccQueueMode_MULTI_QUEUE
/* Initialize the accumulator list memory */
memset ((Void *)&gHiPriAccumList0[corenum], 0, sizeof(gHiPriAccumList0));
drvCfg.u.drvManagedCfg.rxCfg.accCfg.listAddress = l2_global_address((UInt32)&gHiPriAccumList0[corenum]);
}
/* Driver Managed: Transmit Configuration */
drvCfg.u.drvManagedCfg.bIsTxCfgValid = 1;
drvCfg.u.drvManagedCfg.txCfg.txMemRegion = Qmss_MemRegion_MEMORY_REGION1;//Qmss_MemRegion_MEMORY_REGION0
drvCfg.u.drvManagedCfg.txCfg.numTxBuffers = 4;
drvCfg.u.drvManagedCfg.txCfg.txMTU = SRIO_MAX_MTU;
/* Start the Driver Managed SRIO Driver. */
hDrvManagedSrioDrv = Srio_start(&drvCfg);
if (hDrvManagedSrioDrv == NULL)
{
System_printf ("Error(Core %d): SRIO Driver failed to start\n", corenum);
return -1;
}
/* Enable Time Stamp Counter */
CSL_tscEnable();
int32_t eventId;
UInt8 LSU_Int_HostIntNum;
/* Get the CSL SRIO Handle. */
hSrioCSL = CSL_SRIO_Open (0);
if (hSrioCSL == NULL)
return -1;
//映射LSU TX完成中断
LSU_Int_HostIntNum = 8+corenum+16*corenum;
CSL_SRIO_DisableInterruptPacing (hSrioCSL, corenum);
CSL_SRIO_RouteLSUInterrupts (hSrioCSL, corenum, corenum);
CpIntc_dispatchPlug(CSL_INTC0_INTDST0+corenum, (CpIntc_FuncPtr)myDioTxCompletionIsr, (UArg)hDrvManagedSrioDrv, TRUE);
CpIntc_mapSysIntToHostInt(0, CSL_INTC0_INTDST0+corenum, LSU_Int_HostIntNum);
CpIntc_enableHostInt(0, LSU_Int_HostIntNum);
CpIntc_enableSysInt(0, CSL_INTC0_INTDST0+corenum);
eventId = CpIntc_getEventId(LSU_Int_HostIntNum);
EventCombiner_dispatchPlug (eventId, CpIntc_dispatch, LSU_Int_HostIntNum, TRUE);
//映射LSU TX失败中断
LSU_Int_HostIntNum = 12+corenum+16*corenum;
CSL_SRIO_DisableInterruptPacing (hSrioCSL, corenum+4);
CSL_SRIO_RouteLSUInterrupts (hSrioCSL, corenum+16, 4+corenum);
CpIntc_dispatchPlug(CSL_INTC0_INTDST0+corenum+4, (CpIntc_FuncPtr)myDioTxErrorIsr, (UArg)hDrvManagedSrioDrv, TRUE);
CpIntc_mapSysIntToHostInt(0, CSL_INTC0_INTDST0+corenum+4, LSU_Int_HostIntNum);
CpIntc_enableHostInt(0, LSU_Int_HostIntNum);
CpIntc_enableSysInt(0, CSL_INTC0_INTDST0+corenum+4);
eventId = CpIntc_getEventId(LSU_Int_HostIntNum);
EventCombiner_dispatchPlug (eventId, CpIntc_dispatch, LSU_Int_HostIntNum, TRUE);
EventCombiner_dispatchPlug (20, (CpIntc_FuncPtr)myDorrbellFunc, (UArg)hDrvManagedSrioDrv, TRUE);
return 0;
然后SRIO发送Doorbell的代码如下:
bindInfo.dio.doorbellValid = 0;
bindInfo.dio.intrRequest = 1;
bindInfo.dio.supInt = 0;
bindInfo.dio.xambs = 0;
bindInfo.dio.priority = 0;
//bindInfo.dio.outPortID = 3;//for 1X port3
bindInfo.dio.outPortID = 0;//for 4X port0
bindInfo.dio.idSize = 0;
bindInfo.dio.srcIDMap = corenum;
bindInfo.dio.hopCount = 0;
bindInfo.dio.doorbellReg = 0;
bindInfo.dio.doorbellBit = 0;
if (Srio_sockBind_DIO (srioSocket[corenum], &bindInfo) < 0)
{
System_printf ("Error: Binding the SIO socket failed.\n");
return -1;
}
/*********************************************************************************
* Run multiple iterations of the example to ensure multiple data transfers work
*********************************************************************************/
if(dio_ftype == Srio_Ftype_DOORBELL)
{
//见Keystone SRIO手册的Figure2-22
if(corenum == 0)
doorbellInfo = SRIO_SET_DBELL_INFO(0,6);
else if(corenum == 1)
doorbellInfo = SRIO_SET_DBELL_INFO(1,6);
else if(corenum == 2)
doorbellInfo = SRIO_SET_DBELL_INFO(2,6);
else if(corenum == 3)
doorbellInfo = SRIO_SET_DBELL_INFO(3,6);
else
{
System_printf("Doorbell Info set error!\n");
return -1;
}
/* Populate the DIO Address Information where the data is to be sent. */
to.dio.rapidIOMSB = 0x0;
to.dio.rapidIOLSB = (uint32_t)READ_BASE_ADDR;
to.dio.dstID = DEVICE_DST_ID; //DEVICE_ID2_16BIT;
to.dio.ttype = dio_ttype;
to.dio.ftype = dio_ftype;
if (Srio_sockSend_DIO (srioSocket[corenum],(Srio_DrvBuffer)doorbellInfo, 0, (Srio_SockAddrInfo*)&to) < 0)
{
System_printf ("DIO Socket Example Failed\n");
return -1;
}
while(! srioLsuIsrServiced);
/* Read the completion code filled by the ISR */
compCode = 0xFF;
if (Srio_getSockOpt(srioSocket[corenum], Srio_Opt_DIO_READ_SOCK_COMP_CODE, &compCode, sizeof(uint8_t)) < 0)
{
System_printf ("Error: Unable to read the completion code in socket\n");
return -1;
}
//System_printf("Completition Code is %d\n",compCode);
CSL_SRIO_ClearDoorbellPendingInterrupt (hSrioCSL, corenum, 0xFFFF);
CSL_SRIO_ClearLSUPendingInterrupt (hSrioCSL, 0xFFFFFFFF, 0xFFFFFFFF);
srioLsuIsrServiced = 0;
System_printf ("SRIO Doorbell Operation OK!\n");
}
************************************************************************************************
遇到的问题是:
Core0一切正常,能够对外发送Doorbell包,但是Core1~Core3没发送一个Doorbell包,就卡在
while(! srioLsuIsrServiced);
就是说Core1~Core3在发送Doorbell包的时候,LSU没有正常进入TXComletionIsr。
************************************************************************************************
经过测试,4个Core加载代码,同时对外发送Doorbell包,结果如下
1. Core0上:每发送一次Doorbell包,LSU3_stat0~LSU3_stat3依次0、1变化,
Core0能够进入ICS0 – SRCID0, Transaction complete, No Errors (Posted/Non-posted)中断
2. Core1上:每发送一次Doorbell包,LSU0_stat0~LSU0_stat3依次2、3变化
Core1进入ICS17 – SRCID1, Transaction complete with error中断
3. Core2上:每发送一次Doorbell包,LSU1_stat0~LSU1_stat3依次2、3变化
Core2进入ICS18 – SRCID2, Transaction complete with error中断
4. Core3上:每发送一次Doorbell包,LSU2_stat0~LSU2_stat3依次2、3变化
Core3进入ICS19 – SRCID3, Transaction complete with error中断
顺便贴上LSUx_staty的寄存器值表格
应该是Core1~Core3在发送Doorbell包的时候,遇到了0b001 Timeout问题,所以无法进入myDioTxCompletionIsr中断处理函数,而进入了myDioTxErrorIsr中断处理函数。
可是这样的代码在Core0上运行无误,而且我测试如果4个Core对外发送的不是Doorbell而是SWRITE包,也不会发生这种Core1~Core3 LSU Transaction Timeout的问题。
************************************************************************************************
希望大家能帮我分析一下~~非常感谢