This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于6678开发板的DDR初始化问题



Hi,all!

试着用DDR3配置参数的Excel(DDR3 PHY Calc v10)来验证STK代码中的DDR3初始化配置。

发现:

1.原理图中6678控制器的DDRCLKOUTP0时钟信号,外接了电阻和电容,但是在PCB上,并未看到有这两个阻容。

2.在DDR3 Initialization文档中,提到6678 EVM的DDR3配置值,这些值即是DDR3 PHY Calc v10 Excel的初始化值。

但是,实际去测量了下6678EVM PCB,发现DQS的inch能对上,但是CK的inch却对不上。实际测量值要小些。不知道这个是怎么回事?

另外,Excel中提到要区别microstrip和stripline两者的长度,在PCB中也看到有microstrip的走线,但是实际配置时,都是按照stripline来配置了。

3.Excel生成的_Init_Ratio值,与STK开发包中提供的C6678_EVM_DDR_Init函数中的实际配置值又是不一样的。


麻烦TI工程师给确认下这几个问题,谢谢!