This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCC AWB无法调试的问题



强大的TI工程师,你好:

在使用DCC调试AWB时,由于暂时没有灯箱,所以我在reference files选择了5张相同环境下的RAW图像,然后Additional references都是使用DCC自带的色卡图,然后点击调试,在消息窗口中出现如下提示:

Plugin returned message:
No flash has not yet been tuned, default params loaded.
Please load all reference files for No flash, then go to the next step.

H3A Info:
----------------------------
Paxel Sizes: 64 H, 8 V
Paxel Counts: 30 H, 128 V
Start Offset: 0 H, 30 V
Decimation: NO

这是选择的reference files图片

请问一下为什么无法成功进行白平衡调试呢?谢谢!!!