Other Parts Discussed in Thread: TPS65950, DM3730
如题,现用DM3730设计,计划不使用TI推荐的TPS65950等相关PMIC,不知道ARM跟DSP的性能能否达到最高的速度及显示最强的性能?还有就是vdd_mpu_iva和vdd_core的电压给多大?是不是SmartReflex ,DVFS,AVS这些省电的功能全没了?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
processors.wiki.ti.com/.../DM37x_Overview
请在这里选择需要的PMIC,如果要3730 1G主频arm dsp完全使用,需要1.4A的支持.
一定要用PMIC因为3730上电的时候就会通过i2c和pmic通讯.
不一定使用PMU来完成,使用离散的DC-DC都可以,但需要控制好上电时序 ,IP camera 不需要SmartReflex 功能,
分散的DC-DC直接输出1G主频所需的稳定的电压。
www.tianyeit.com
从datasheet看,关键调的是vdd1的电压,也就是vdd_mpu_iva的电压,你可以按照datasheet上要求的电压上电时序和电压,电流等要求,进行电源设计,至于哪个便宜,这个要你自己来算了