内核已经打印出这样的信息:
说明三个串口的驱动是没问题的。
可是在应用层中的测试程序打开ttyS0和ttyS1后,收不到数据,也发不出数据。不知道为啥会这样!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
omap-l138 mcdk linux kernel bad on ttyS1
遇到同样问题, 请问如何解决ttyS1 不能收发数据的问题? 我用的内核是psp03.22.00.06.sdk中的 linux-3.3. 谢谢.
我已经改动如下
First you need to setup pinmuxing for UART1. Add these lines at in board-da850evm.c:
static const short da850_evm_uart_pins[] = {
DA850_UART1_RXD, DA850_UART1_TXD,
-1
};
and in the da850_evm_init() function add
ret = davinci_cfg_reg_list(da850_evm_uart_pins);
if (ret)
pr_warning("da850_evm_init: uart mux setup failed: %d\n", ret);
The da850_evm_init() function disables all UARTs that are not used in Linux (currently UART 0 and UART 1). So you must modify it so UART1 does not get disabled. Comment out this code:
/* __raw_write(0, IO_ADDRESS(DA8XX_UART1_BASE) + 0x30); */
相同问题: http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/168896
楼上的哥们儿:
首先要确保你用的串口是打开的:
static struct davinci_uart_config da850_evm_uart_config __initdata = {
.enabled_uarts = 0x7,
};
其次,在3.3内核中应该是一个bug,必须要添加:
__raw_writel(0x00006000, IO_ADDRESS(DA8XX_UART0_BASE) + 0x30); __raw_writel(0x00006000, IO_ADDRESS(DA8XX_UART1_BASE) + 0x30);
而在3.8内核中是不需要这样的。
刚才回你邮件发布出去,特意来论坛回帖,试一下吧,祝你好运。