Hi,
我用的是DM8127,IPNC RDK 3.8。我修改了ENC_A8_DEC usecase,想保存H264流文件到本地。结果大约保存了2500帧左右,线程会阻塞很久,然后才会继续执行,请问是什么原因?
代码如下:
Void *MultiCh_ipcBitsMain(Void *prm)
{
UInt32 i;
OSA_DmaCopy1D copy1D;
Bitstream_BufList fullBitsBufList;
Bitstream_BufList emptyBitsBufList;
IpcBitsOutLinkHLOS_BitstreamBufReqInfo ipcReqInfo;
OSA_printf("Entered IPC Bits Handler function\n");
gIpcBitsThObj.exitTh = FALSE;
gIpcBitsThObj.exitDone = FALSE;
//unsigned char const start_code[4] = { 0x00, 0x00, 0x00, 0x01 };
FILE *outFile = NULL;
FILE *outFile2 = NULL;
UInt8 *buf = NULL;
UInt32 n = 0;
if(outFile == NULL)
{
outFile = fopen("8127Test.h264", "w");
if (outFile == NULL) {
OSA_printf("Failed to open file for writing\n");
exit(0);
}
}
if(outFile2 == NULL)
{
outFile2 = fopen("8127Test.hdr", "w");
if (outFile2 == NULL) {
OSA_printf("Failed to open file for writing\n");
exit(0);
}
}
while(gIpcBitsThObj.exitTh == FALSE)
{
OSA_semWait(&gIpcBitsNotifySem,OSA_TIMEOUT_FOREVER);
IpcBitsInLink_getFullVideoBitStreamBufs(gIpcBitsInHLOSId,&fullBitsBufList);
if(fullBitsBufList.numBufs > 0)
{
for(i = 0;i < fullBitsBufList.numBufs;i++)
{
ipcReqInfo.numBufs = 1;
ipcReqInfo.minBufSize[0] = DEC_MIN_BUF_SIZE;
/* Wait till empty buffer is got from IPC Bits Out link */
do
{
IpcBitsOutLink_getEmptyVideoBitStreamBufs(gIpcBitsOutHLOSId,&emptyBitsBufList,&ipcReqInfo);
OSA_waitMsecs(10);
}while(emptyBitsBufList.numBufs == 0);
/* Copy bitstream */
emptyBitsBufList.numBufs = 1;
emptyBitsBufList.bufs[0]->channelNum = fullBitsBufList.bufs[i]->channelNum;
emptyBitsBufList.bufs[0]->fillLength = fullBitsBufList.bufs[i]->fillLength;
emptyBitsBufList.bufs[0]->timeStamp = fullBitsBufList.bufs[i]->timeStamp;
if(gDmaHndl.chId == 0xFF)
{
memcpy(emptyBitsBufList.bufs[0]->addr,
(fullBitsBufList.bufs[i]->addr + fullBitsBufList.bufs[i]->startOffset),
fullBitsBufList.bufs[i]->fillLength);
}
else
{
copy1D.srcPhysAddr = (unsigned long)CMEM_getPhys(fullBitsBufList.bufs[i]->addr + fullBitsBufList.bufs[i]->startOffset);
copy1D.dstPhysAddr = (unsigned long)CMEM_getPhys(emptyBitsBufList.bufs[0]->addr);
copy1D.size = fullBitsBufList.bufs[i]->fillLength;
OSA_dmaCopy1D(&gDmaHndl,©1D,1);
}
#if 1
buf = fullBitsBufList.bufs[i]->addr + fullBitsBufList.bufs[i]->startOffset;
if (fwrite(buf, fullBitsBufList.bufs[i]->fillLength, 1, outFile) != 1) {
OSA_printf("Failed to write data to file\n");
exit(0);
}
#endif
fprintf(outFile2, "%d, ", fullBitsBufList.bufs[i]->fillLength);
n++;
if(n % 100 == 0)
OSA_printf("received %d frames.\n", n);
if(n == 3000)
{
fclose(outFile);
fclose(outFile2);
exit(0);
}
IpcBitsOutLink_putFullVideoBitStreamBufs(gIpcBitsOutHLOSId,&emptyBitsBufList);
}
}
IpcBitsInLink_putEmptyVideoBitStreamBufs(gIpcBitsInHLOSId,&fullBitsBufList);
}
gIpcBitsThObj.exitDone = TRUE;
OSA_printf("Exiting IPC Bits Handler function\n");
return NULL;
}
log如下:
Starting syslogd/klogd: done
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org DM8127_IPNC ttyO0
Arago 2011.09 DM8127_IPNC ttyO0
DM8127_IPNC login: root (automatic login)
root@DM8127_IPNC:~# mkdosfs 3.0.12 (29 Oct 2011)
unable to get drive geometry, using default 255/63
/dev/sbulla has 255 heads and 63 sectors per track,
logical sector size is 512,
using 0xf8 media descriptor, with 1024 sectors;
file system has 2 12-bit FATs and 4 sectors per cluster.
FAT size is 1 sector, and provides 247 clusters.
There is 1 reserved sector.
Root directory contains 512 slots and uses 32 sectors.
Volume ID is 63107077, no volume label.
g_file_storage gadget: No serial-number string provided!
g_file_storage gadget: File-backed Storage Gadget, version: 1 September 2010
g_file_storage gadget: Number of LUNs=1
g_file_storage gadget-lun0: ro=0, nofua=0, file: /dev/sbulla
[m3vpss ] CT: 5592, 3dlut index:2
Simple mixer control 'PGA',0
Capabilities: cvolume cswitch penum
Capture channels: Front Left - Front Right
Limits: Capture 0 - 119
Front Left: Capture 80 [67%] [40.00dB] [on]
Front Right: Capture 80 [67%] [40.00dB] [on]
queue id:0
[m3vpss ] CT: 6091, 3dlut index:3
[host] received 100 frames.
./boa: /usr/lib/libssl.so.1.0.0: no version information available (required by ./boa)
./boa: /usr/lib/libcrypto.so.1.0.0: no version information available (required by ./boa)
ApproDrvInit: 3
queue id:163845
queue id:0
queue id:32769
queue id:0
[host] received 200 frames.
[host] received 300 frames.
[host] received 400 frames.
[host] received 500 frames.
[host] received 600 frames.
TimeOut occure in boot_proc.
Program exit.
[host] received 700 frames.
TimeOut occure in boot_proc.
Program exit.
[host] received 800 frames.
[host]
Usecase is Active !!!
[host] received 900 frames.
[host] received 1000 frames.
[host] received 1100 frames.
[host] received 1200 frames.
[host] received 1300 frames.
[host] received 1400 frames.
[host] received 1500 frames.
[host] received 1600 frames.
[host] received 1700 frames.
[m3vpss ] 66182: CAMERA: Fields = 1801 (fps = 30), Total Resets = 0 (Avg 0 ms per reset)
[m3video] ==================== EncLink_PrintDetails ====================
[m3video] 67020: HDVICP-ID:0
[m3video] totalAcquire2wait in msec: 1125
[m3video] totalWait2Isr in msec: 45929
[m3video] totalIsr2Done in msec: 65
[m3video] totalWait2Done in msec: 45994
[m3video] totalDone2Release in msec: 0
[m3video] totalAcquire2Release in msec: 47715
[m3video] totalAcq2acqDelay in msec: 13053
[m3video] totalElapsedTime in msec: 60767
[m3video] numAccessCnt: 3567
[m3video] IVA-FPS : 59
[m3video]
[m3video] *** ENCODE Statistics ***
[m3video]
[m3video] Elasped Time : 60 secs
[m3video]
[m3video]
[m3video] CH | In Recv In Skip In User Out Latency
[m3video] Num | FPS FPS Skip FPS FPS Min / Max
[m3video] --------------------------------------------
[m3video] 0 | 30 0 0 29.67 14 / 56
[m3video]
[m3video] Multi Channel Encode Average Submit Batch Size
[m3video] Max Submit Batch Size : 24
[m3video] IVAHD_0 Average Batch Size : 1
[m3video] IVAHD_0 Max achieved Batch Size : 1
[m3video] ==============================================================
[host]
Usecase is Active !!!
[host] received 1800 frames.
[host] received 1900 frames.
ApproDrvExit: 7
Error: WaitStreamReady Fail.
Error: SemWait: Invalid Semaphore handler
Error: SemRelease: Invalid Semaphore handler
Error: SemWait: Invalid Semaphore handler
[host]
Force IDR on Channel: 0
[host]
Force IDR on Channel: 1Error: SemRelease: Invalid Semaphore handler
SystemInit success
Schedule manager init success
Dmva Schedule manager init success
umount: can't umount /mnt/mmc: Invalid argument
killall: dhcpcd: no process killed
rm: cannot remove '/var/run/dhcpcd-eth0.pid': No such file or directory
[host] received 2000 frames.
[host] received 2100 frames.
[host] received 2200 frames.
[host] received 2300 frames.
[host] received 2400 frames.
[host] received 2500 frames.
[host]
Usecase is Active !!!
[m3vpss ] ==================== CameraLink_PrintDetails ====================
[m3vpss ] 126123: CAMERA: Fields = 3601 (fps = 30, CPU Load = 27)
[m3vpss ] 126123: CAMERA: Num Resets = 0 (Avg 0 ms per reset)
[m3vpss ] =================================================================
[m3vpss ] 126189: CAMERA: Fields = 1801 (fps = 30), Total Resets = 0 (Avg 0 ms per reset)
[host]
Usecase is Active !!!
[host]
Usecase is Active !!!
[m3video] ==================== EncLink_PrintDetails ====================
[m3video] 161645: HDVICP-ID:0
[m3video] totalAcquire2wait in msec: 1618
[m3video] totalWait2Isr in msec: 65598
[m3video] totalIsr2Done in msec: 80
[m3video] totalWait2Done in msec: 65678
[m3video] totalDone2Release in msec: 0
[m3video] totalAcquire2Release in msec: 68152
[m3video] totalAcq2acqDelay in msec: 18103
[m3video] totalElapsedTime in msec: 86242
[m3video] numAccessCnt: 5095
[m3video] IVA-FPS : 59
[m3video]
[m3video] *** ENCODE Statistics ***
[m3video]
[m3video] Elasped Time : 94 secs
[m3video]
[m3video]
[m3video] CH | In Recv In Skip In User Out Latency
[m3video] Num | FPS FPS Skip FPS FPS Min / Max
[m3video] --------------------------------------------
[m3video] 0 | 30 22 0 8.14 14 / 29
[m3video]
[m3video] Multi Channel Encode Average Submit Batch Size
[m3video] Max Submit Batch Size : 24
[m3video] IVAHD_0 Average Batch Size : 1
[m3video] IVAHD_0 Max achieved Batch Size : 1
[m3video] ==============================================================
net_search_gateway:eth0, 1A8C0, 0, 1
dns=192.168.1.1
net_search_gateway:eth0, 1A8C0, 0, 1
net_search_gateway:eth0, 0, FE01A8C0, 3
dns=192.168.1.1
g_file_storage gadget: No serial-number string provided!
g_file_storage gadget: File-backed Storage Gadget, version: 1 September 2010
g_file_storage gadget: Number of LUNs=1
g_file_storage gadget-lun0: ro=0, nofua=0, file: /dev/sbulla
[09/Nov/2012:12:25:24 +0000] boa: server version Boa/0.94.13
[09/Nov/2012:12:25:24 +0000] boa: server built Aug 19 2014 at 09:27:37.
[09/Nov/2012:12:25:24 +0000] boa: starting server pid=549, port 80
queue id:0
<UDN>uuid:Upnp-TVEmulator-1_0-00_0095591997</UDN>
Upnp port is 0
UPnP Initialized OK ip=192.168.1.224, port=0
desc_doc_url = 192.168.1.224/tvdevicedesc.xml
error code = 0
device advertisement succeed.
queue id:131076
ApproDrvInit: 10
queue id:163845
Initializing...
...done initializing
Play this stream using the URL:
rtsp://192.168.1.224:8557/PSIA/Streaming/channels/2?videoCodecType=H.264
(We use port 8304 for optional RTSP-over-HTTP tunneling.)
ApproDrvInit: 6
queue id:163845
Initializing...
...done initializing
Play this stream using the URL:
rtsp://192.168.1.224:8554/PSIA/Streaming/channels/1?videoCodecType=MPEG4
(We use port 8301 for optional RTSP-over-HTTP tunneling.)
ApproDrvInit: 2
ApproDrvInit: 8
queue id:163845
Initializing...
...done initializing
Play this stream using the URL:
rtsp://192.168.1.224:8555/PSIA/Streaming/channels/0?videoCodecType=MJPEG
(We use port 8302 for optional RTSP-over-HTTP tunneling.)
ApproDrvInit: 9
queue id:163845
Initializing...
...done initializing
Play this stream using the URL:
rtsp://192.168.1.224:8553/PSIA/Streaming/channels/1?videoCodecType=MPEG4
(We use port 8300 for optional RTSP-over-HTTP tunneling.)
queue id:163845
Initializing...
...done initializing
Play this stream using the URL:
rtsp://192.168.1.224:8556/PSIA/Streaming/channels/2?videoCodecType=H.264
(We use port 8303 for optional RTSP-over-HTTP tunneling.)
[host] received 2600 frames.
[host] received 2700 frames.
[host] received 2800 frames.
[host] received 2900 frames.
[host] received 3000 frames.
[m3vpss ] 186197: CAMERA: Fields = 1801 (fps = 30), Total Resets = 0 (Avg 0 ms per reset)