如题,将HDVPSS的输入口设置为24bit的RGB输入方式,是不是输入时钟低于165MHz的所有的符合VESA标准的 RGB数字信号数据输入,HDVPSS都能支持呢?例如1280X1024 @ 85fps,1920X1080 @ 60fps,和1600X1200 @ 60fps三种RGB输入格式是否都支持呢?配置输入端口的参数的相关驱动部分都有哪些驱动文件?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题,将HDVPSS的输入口设置为24bit的RGB输入方式,是不是输入时钟低于165MHz的所有的符合VESA标准的 RGB数字信号数据输入,HDVPSS都能支持呢?例如1280X1024 @ 85fps,1920X1080 @ 60fps,和1600X1200 @ 60fps三种RGB输入格式是否都支持呢?配置输入端口的参数的相关驱动部分都有哪些驱动文件?
追问:
Technical Reference Manual上说,I/O域时钟的HDVPSS部分的VIN[0]A_CLK, VIN[0]B_CLK,VIN[1]A_CLK,VIN[1]B_CLK的输入时钟频率是162MHz,内部系统时钟SYSCLK13, SYSCLK15,SYSCLK17分别是165MHz,165MHz,54MHz。是否说明,对VIP接口的外部输入时钟而言,可以是低于162MHz,并且是27MHz的整数倍的时钟频率就可以啊?即27,54,81,108,135,162MHz都可以啊;或者是使用与SYSCLK13, SYSCLK15,SYSCLK17同频率的165MHz和54MHz的就行啊?请您说的详细点。谢谢啦
另外,如果我的输入是一个非标准的视频信号,例如分辨率1024X1024 帧频60fps数据格式RGB 24bit时钟80MHz,该输入能否被DM8168正确读取?如果不能是因为时钟不是27MHz的整数倍吗?
期待您的回复!谢谢啦
如果方便的话请把邮箱告诉下,谢谢啦
我的邮箱 zyrbeyond@163.com