This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDR3 narrow mode error issue on the DM385 IPNC Kit



Dear all,

我們想要在DM385 IPNC reference design kit上改用NARROW mode,將DDR3的Data bus width由32 bits改成16 Bits。

我們把原本DDR3(533MHz)之中的參數SDRCR(DDR3_EMIF_SDRAM_CONFIG)設定由0x61C11A32改成0x61C15A32。

在IPNC kit上執行Pre-build的uImage與UBIFS時,會產生Timeout Error(如下)而無法開機。

Simple mixer control 'PGA',0
Capabilities: cvolume cswitch penum
Capture channels: Front Left - Front Right
Limits: Capture 0 - 119
Front Left: Capture 80 [67%] [40.00dB] [on]
Front Right: Capture 80 [67%] [40.00dB] [on]
queue id:0
ApproDrvInit: 3
Creat queue id:131076
queue id:131076
queue id:0
ApproDrvInit: 7
queue id:131076
TimeOut occure in boot_proc.
Program exit.
TimeOut occure in boot_proc.
Program exit.