This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

自己做的板子,为什么运行不了程序呢?

Other Parts Discussed in Thread: OMAP-L138

刚做好的OMAPL138的板子,第一个程序跑步起来。进不了main函数。点击suspend后,弹出来一个0xFFFF0004的子窗口。

新手请教是什么原因呢?

今天发现了这个错误:

ARM9_0: Output:     Memory Map Cleared.
ARM9_0: Output:     ---------------------------------------------
ARM9_0: Output:     Memory Map Setup Complete.
ARM9_0: Output:     ---------------------------------------------
ARM9_0: Output:     Enabling Experimenter PSCs...
ARM9_0: Output:     PSC Enable Complete.
ARM9_0: Output:     ---------------------------------------------
ARM9_0: GEL: Error while executing OnTargetConnect(): Target failed to write 0x01C11138     at (*((unsigned int *) (0x01C11000+0x138))|=0x1) [EXPKITOMAPL138_ARM.gel:25]     at device_PLL0(0, 24, 1, 0, 1, 11, 5) [EXPKITOMAPL138_ARM.gel:405]     at Set_Core_300MHz() [EXPKITOMAPL138_ARM.gel:464]     at Core_300MHz_mDDR_150MHz() [EXPKITOMAPL138_ARM.gel:252]     at OnTargetConnect() .