This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6748问题



我使用的是广州创龙的开发板,有几个问题需要请教一下:

1. 开发板提供的GEL文件CPU频率有456MHz,开发文档中也有说明,1.3V下频率可以达到456MHz。

请问在配置Global Settings时,CPU Speed In MHz是否也应该改为456?

2. The device DSP core uses a 2-level cache-based architecture. The level 1 program cache (L1P) is a 32-KB direct mapped cache, and the level 1 data cache (L1D) is a 32-KB 2-way, set-associative cache. The level 2 program cache (L2P) consists of a 256-KB memory space that is shared between program anddata space. L2 memory can be configured as mapped memory, cache, or combinations of the two.    二级缓存可以配置成cache或RAM,一级缓存也可以吗?

3. Memory 中,有两部分地址都指向L2 ROM,L2 RAM等,如下图所示,请解释一下是什么意思。

  • 1. Global Setting根据你的硬件支持的clock speed设置。

    2. 一级cache也可以配置成cache或者RAM.

    3.这两块RAM/ROM其实对应的是同一块物理memory, 它们的区别是0x00800000/0x00700000处的这块L2 RAM/ROM只能DSP访问 而另外一块0x11800000/0x11700000 L2 RAM/ROM则可以被DSP, EDMA, PRUSS以及Master Peripherals访问, 可以参考数据手册上的Table 2-4. C6748 Top Level Memory Map.