This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am1808适用的ddr2芯片

Other Parts Discussed in Thread: AM1808

您好,am1808外接的ddr2芯片,我们选的型号是K4T51163QG-HCF7,具体参数是DDR2-8---6-6-6

CL的值是6,而1808要求的CL,最大是CL=5.

我有些疑惑,ddr2的这个cl参数是可编程的,可以选择2,3,4,5,6呢,还是芯片参数CL是固定的6.

现在感觉DDR2有些不可能。虽然我的测试扫描程序可以通过。不知道是不是这个原因。

  • 焦急等待中,请TI的工程师给予答疑解惑。谢谢。

  • CL是可编程的。

    下图是DDR手册中拷贝出来的参数表。如中间一例与你所选用的DDR参数一样。它可以支持CL=4,5,6,在不同的CL值下,所能支持的最高速度不一样,要工作在400MHz(2.5ns)即DDR2-800,必须设置CL=6,在CL=5时,DDR_CLK的范围在3ns~8ns, 即125MHz~333MHz。

    同时可以注意到所有模式下,DDR_CLK最大为8ns,即DDR2支持的最低频率为125MHz。