This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6455 mcbsp配置为串口通讯问题

Other Parts Discussed in Thread: TMS320C6455

芯片:TMS320C6455

描述 :通过DSP 的MCBSP配置为232串口,与PC进行通信。DSP的发送采用中断的方式。

         中断函数如下:

          //发送中断

void SerialPortSendInt()

{

CSL_mcbspWrite (hMcbsp, CSL_MCBSP_WORDLEN_16, &xmitbuf[sendCount]);

sendCount++;

if(sendCount == NUM)

{

//发送标志

sendCount = 0;

semFlag = MCBSP_SEND;

SEM_post(&SEM_MCBSP_RECE);

  }

}

经过测试,可以与pc正常通讯。

问题:*************************

 我在上面的程序基础上增加了一个GPIO中断,用来做数据采集。GPIO中断优先级高于串口发送中断。增加后,串口通信出现异常。主要表现为:最高位经常翻转。例如本来是00000000,接收到却是10000000.不知是何原因。

我将两个的优先级调换后,还是出现此问题。有没有人遇到相通的问题,请教!