This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352 spec 中电压问题



参考附件 我下载的文档,section5.5 P85中,VDDSHV1-6 这几个电压为何既可以是1.8V,也有3.3V描述?

是不是可以软件配置呢?如果是这样,具体如何配置?

 

am3352.pdf
  • 这几个I/O口是属于dual-voltage I/O domain,既可以1.8V又可以3.3V。印象中这个不是软件配置,而是你硬件的接法,这个东西会决定你VDDSHV1~6对应的I/O域值电压。举个例子,P22的table4-1,其中GPMC_A0,后面的power域中显示其属于VDDSHV3域,如果VDDSHV3=1.8,所以这个管脚在使用的时候,电压的范围是在1.8V域内的。如果VDDSHV3=3.3,这个管脚的电压范围在3.3V域内。

  • 建议你下一个pinmux工具,上面的每个管脚的电压描写得很清楚