我的C6455配置接收缓冲区大小为8192
//
// This code sets up the TCP and UDP buffer sizes
// (Note 8192 is actually the default. This code is here to
// illustrate how the buffer and limit sizes are configured.)
//
// UDP Receive limit
rc = 8192;
CfgAddEntry( hCfg, CFGTAG_IP, CFGITEM_IP_SOCKUDPRXLIMIT,
CFG_ADDMODE_UNIQUE, sizeof(uint), (UINT8 *)&rc, 0 );
然后开启守护进程:
hHello = DaemonNew( SOCK_DGRAM, 0, 7, dtask_udp_hello,
OS_TASKPRINORM, OS_TASKSTKNORM, 0, 1 );
接收如下:
count = (int)recvncfrom( s, (void **)&p_Buf, 0, (PSA)&sin1, &tmp, &hBuffer );
问题如下:
每次我只能收512字节数据,有时候能收513,我一帧数据有6000多,一次不能收完全接收,要分多次接收,这是怎么回事?明明缓冲区分配了8192,一次收6000应该没问题啊????大神呢????