hal_eth_c6455.lib,请问,我修改了源程序,怎么新建这个hal_eth_c6455.lib库?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
rc = 8192;
CfgAddEntry( hCfg, CFGTAG_IP, CFGITEM_IP_SOCKUDPRXLIMIT,
CFG_ADDMODE_UNIQUE, sizeof(uint), (UINT8 *)&rc, 0 );
那么这里的8192不就设置没用,这个缓冲区限制的是什么大小?
getsockopt(s, SOL_SOCKET, SO_RCVBUF, (char*)&optVal, &optLen);
通过这个调用,可以看到缓冲区大小也是8192啊我找到了下面链接,参考一下这里的设置方法:
http://processors.wiki.ti.com/index.php/NDK_Dynamic_Memory_Manager#Sockets