请教各位,
我现在想通过dm368的boa web sever进行固件更新,但是我升级rootfs的说话,会出现 No space left on device,升级kernel可以。
rootfs有38M,kernel只有4M。
是不是内存不够了?如何修改,请教下各位。
出错打印如下:
[01/Jan/1970:00:00:57 +0000] read.c:379 - read 20480 bytes.
[01/Jan/1970:00:00:57 +0000] read.c:433 - wrote 20480 bytes. 26091082 of 36700476
[01/Jan/1970:00:00:57 +0000] read.c:379 - read 20480 bytes.
[01/Jan/1970:00:00:57 +0000] read.c:433 - wrote 20480 bytes. 26111562 of 36700476
[01/Jan/1970:00:00:57 +0000] read.c:379 - read 20480 bytes.
[01/Jan/1970:00:00:57 +0000] read.c:433 - wrote 20480 bytes. 26132042 of 36700476
[01/Jan/1970:00:00:57 +0000] read.c:379 - read 20480 bytes.
[01/Jan/1970:00:00:57 +0000] read.c:433 - wrote 438 bytes. 26152522 of 36700476
[01/Jan/1970:00:00:57 +0000] request from 192.168.2.107 "POST /update.cgi HTTP/1.1" ("/var/www/update.cgi"): write body: No space left on device
[01/Jan/1970:00:00:57 +0000] buffer.c:229 - Wrote "HTTP/1.0 500 Server Error
系统的meminfo是:
root@192:~# cat /proc/meminfo
MemTotal: 44644 kB
MemFree: 26572 kB
Buffers: 24 kB
Cached: 7816 kB
SwapCached: 0 kB
Active: 4924 kB
Inactive: 6520 kB
Active(anon): 3636 kB
Inactive(anon): 288 kB
Active(file): 1288 kB
Inactive(file): 6232 kB
Unevictable: 0 kB
Mlocked: 0 kB
SwapTotal: 0 kB
SwapFree: 0 kB
Dirty: 20 kB
Writeback: 0 kB
AnonPages: 3632 kB
Mapped: 4652 kB
Shmem: 320 kB
Slab: 2356 kB
SReclaimable: 380 kB
SUnreclaim: 1976 kB
KernelStack: 744 kB
PageTables: 944 kB
NFS_Unstable: 0 kB
Bounce: 0 kB
WritebackTmp: 0 kB
CommitLimit: 22320 kB
Committed_AS: 363380 kB
VmallocTotal: 968704 kB
VmallocUsed: 117228 kB
VmallocChunk: 829436 kB