This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678 SRIO链路信号完整性测试方法



        我已经研究过K1_STK中的SRIO例程,对SRIO的工作方式也很熟悉。现在将DSP板与FPGA板两板通过SRIO 4x进行背板连接,因为FPGA有专门的工具可以通过发送PRBS,然后通过外部物理连接回环TX-->RX测试误码率来验证链路的信号完整性,所以我想进行如下测试:

        测试路径: FPGA --> DSP SRIO SerDes  --> FPGA

        1、STK中的external line loopback工作方式好像满足我的需求,但似乎前提是连接双方必须在SRIO协议基础上建立物理层的连接才可以进行测试。由于FPGA端              并未建立SRIO协议,仅仅通过收发器发送PRBS,在这种情况下是否能使用external line loopback方式来测试链路的信号完整性?

        2、查看手册中的SerDes配置部分,发现TX和RX都有loopback的选项,但例程中是在SerDes loopback方式时才使能了两个选项,这时是DSP的内部回环。我                  能否通过SerDes的loopback选项实现上述的测试方法?

        3、有更简单易行的测试方法吗?