This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6670 MAC地址的问题



大家好,

 

用NDK的例程,C6670的MAC是软件可配置的。

想问一下:

1. 每片C6670在出厂时,是否都固化了一个唯一的MAC地址?C6670有两个SGMII接口,每个SGMII接口都固化了一个唯一的MAC地址吗?如果是,哪个寄存器指示这个MAC地址的值? 

2. 还是说C6670就是没有固化唯一的MAC地址,MAC地址就是通过软件配置的?

 

谢谢!