我将CCS3.3的工程导入CCS5.2中,选项选择的是legacy CCSv3.3 Projects ,但是编译出错,都是E:\ti\ccsv5\tools\compiler\c6000_7.3.4\include路径下报错,我查看了一下,不是头文件,是一个叫exception的文件,然后我把这个路径取消后,又会报错别的头文件无法打开,请问v5导入3.3需要进行什么转换吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我将CCS3.3的工程导入CCS5.2中,选项选择的是legacy CCSv3.3 Projects ,但是编译出错,都是E:\ti\ccsv5\tools\compiler\c6000_7.3.4\include路径下报错,我查看了一下,不是头文件,是一个叫exception的文件,然后我把这个路径取消后,又会报错别的头文件无法打开,请问v5导入3.3需要进行什么转换吗
Description Resource Path Location Type
<a href="file:/E:/ti/ccsv5/tools/compiler/dmed/HTML/5.html">#5</a> could not open source file "windows.h" newdibcom7070 line 8, external location: F:\ODU_MT_U6_DSPy\include\platform\platform_dibcom.h C/C++ Problem
都是类似的问题
我将相关东西删除后,再重新安装了一遍软件,编译通过了,可以连接上硬件,现在想请问一下,在CCS5下怎么将程序烧写到flash里面,有个flashburn可以烧写,但是只支持CCS3.3,在5下怎么烧写呢,有没有相关参考文档,谢谢!
是DSK板的话,可以用flashburn免费版。
如果是自己的板子的话,需要购买flashburn porting kit.
http://www.softwaredesignsolutions.com/flashburn4.aspx
自己写flash烧写flash程序的话,需要根据flash datasheet里的clear/erase/program command来写,google/baidu一下。
你好,我用flashburn4板子可以连接上,但是downloadFBTC时,6416的.out文件是CCS3.3下的,请问在5.2下编译后生成的.out文件还是不能用吗?你们有没有FTBC6416的源代码呢,谢谢!
是下面这个版本吗?这个版本支持CCS v4.2~CCS v5.5.
http://www.softwaredesignsolutions.com/flashburn4.aspx
另外,你用的是DSK6416的话,可以用这个免费版本的flashburn.
在C:\ti\SoftwareDesignSolutions\FlashBurnDSK\examples\DSK6416目录下有FBTCDSK6416.out文件。