This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6670的AIF2和FPGA连接的问题



你好!我们在使用C6670遇到一些问题,希望能够得到您的帮助,问题如下:
在我们的设计中打算使用C6670的AIF接口和一款RF芯片相连。由于RF芯片无法和AIF直接连接,我们在两个片子中间使用了一片FPGA来做适配。在DSP和AIF接口连接时有些疑问:
1、 在使用AIF接口时,是否需要将六对(收发信号)信号,同时连接到FPGA上?(如果需要就需要选择能够支持6对高速口的FPGA芯片来适配。)
2、 在梳理AIF接口信号时除了AIFTX[0:5]P/N和AIFRX[0:5]P/N信号外还有RP1CLKP/N,EXTFRAMEEVENT,RP1FBP/N,PHYSYNC和RADSYNC信号这些信号该如何处理?其中帧同步接口时钟和帧突发指示信号是接到FPGA普通差分对上还是需要接到高速口上?