Other Parts Discussed in Thread: AM3354
该芯片也是支持MII或者RMII接口的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我有个疑问:AM3354上面已经有两个以太网控制器了EMAC,支持MII,RMII,RGMII,只需要外接一个PHY就可以了,为什么还要外接一个以太网控制器芯片呢?
回答你的问题:这部分的驱动应该是没有的,有些客户使用以太网控制器DM9000,和AM335x上的GPMC接口对接,是自己调试的驱动。
AM335x的双网口也是支持switch功能的。
你使用的是Linux吗?如果是的话,可以参考:http://processors.wiki.ti.com/index.php/AM335x_CPSW_(Ethernet)_Driver%27s_Guide
这个驱动,一方面可以到kernel里面看看,另一方面需要跟Dvicom联系了。
看你的描述,感觉2个网口也够用的,我们SK板子是双网口,可以通过执行脚本将其切换成dual mac和NAT模式,不知道你看过下面的guide没有: