你好:
1. 我看到datasheet中这样介绍:
• For address/data-multiplexed and AAD-multiplexed NOR devices, the address is multiplexed on the
data bus.
• 8-bit wide NOR devices do not use GPMC I/O: GPMC_AD[15-8] for data (they are used for address if
needed).
• 16-bit wide NAND devices do not use GPMC I/O: GPMC_A[27-0].
• 8-bit wide NAND devices do not use GPMC I/O: GPMC_A[27-0] and GPMC I/O: GPMC_AD[15-8].
同时 Table 7-5. GPMC Pin Multiplexing Options里也介绍,16bit nandflash地址线与时钟线不用接,但是在 Table 7-5中第二列介绍无复用模式16bit device地址线接A0-A26,数据接AD0-AD15,时钟线也连接上,为什么16bit nandflash就可以不用接地址线与时钟线呢?如果不接怎么知道flash的大小呢?如果换成接16bit 的norflash能不能这样接呢?期待你的回答,谢谢!