您好:
我参考NDK2_20_06_35下的说明文档设置了men.c 和pbm.c。但是其中关于NDK的设置CfgAddEntity和socket的setsocket的代码,应该加在什么地方?是在dtask_UDP_helo还是send()中?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
我参考NDK2_20_06_35下的说明文档设置了men.c 和pbm.c。但是其中关于NDK的设置CfgAddEntity和socket的setsocket的代码,应该加在什么地方?是在dtask_UDP_helo还是send()中?
Hi, 您好!
芯片是支持 jambo packet的, 见GE文档(SPRUGV9C)
Table 3-89 Receive Maximum Length Register (RX_MAXLEN) Field Descriptions
Bits Field Description
31-14 Reserved Reserved
13-0 RX_MAXLEN Reserved Maximum Frame Length. This field determines the maximum length of a received frame. The reset value is 1518
(dec). Frames with byte counts greater than RX_MAXLEN are long frames. Long frames with no errors are oversized frames.
Long frames with CRC, code, or alignment error are jabber frames. The maximum value is 16,383.
在sendto( s, pBuf, i, 0, (PSA)&sin1, sizeof(sin1) );函数中, i表示的是要发送的数据包长度, 您可以尝试把i改大
在dtask_udp_hello函数中, 没有找到有需要修改的地方
谢谢!
Hi, 您好!
您方便描述一下是哪篇文档吗
我查阅了下列文档:
TMS320C6000 Network Developer's Kit (NDK) Software User's Guide (SPRU523G)
TMS320C6000 Network Developer's Kit (NDK) v 2.00 Software Programmer's Reference Guide (SPRU524G)
TMS320C6000 Network Developer's Kit (NDK) Support Package Ethernet Driver Design Guide (SPRUFP2)
没有找到您描述的CfgAddEntity和setsocket, 谢谢
您好 我按照您的说明进行修改,显示错误。我的问题和如下链接相同。http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/t/64374.aspx,
但是我不明白代码楼主描述的代码修改在哪?请能进行详细说明吗?谢谢 楼主说对从某个buffer进行修改可以传输大数据,这个我也不明吧。谢谢您
您好 我按照您的说明只修改了这行代码,但是数据无法传输。
我的问题和http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/t/64374.aspx这个相同。但是我不明白这个楼主的代码修改是怎样的,buffer是那个?
需要重新rebulid ndk 吗?