This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467T网络PHY芯片ET1011C电压异常问题咨询。



原理图设计和官方设计保持一致,ET1011C 的核电压(PHY_1V0)1.0V和PHY层电压(PHY_2V5)2.5V通过外部的两个PNP管生成,单板上电后测试两路电压分别为(PHY_1V0)2.2V和(PHY_2V5)3.2V,与对应的手册不符合,当时其功能正常。然后我们更改设计方案,此两路分别由两个单独的LDO供电,不采用ET1011C自带的单电源方案,(两路LDO分别输出1.0V和2.5V),当单板上电后ET1011C无法工作,测试其LDO输出电流为(PHY_1V0输出0mA/PHY_2V5输出7mA),可以判断此时ET1011C没有工作,当我们手动调节【PHY_1V0】电压至1.7V后([PHY_2V5]保持2.5V不变),BOOT显示已经可以找到PHY(仅仅证明目前MDIO正常),但我们插入网线看网络连接是否正常时去发现无线检查网线的接入(是否可以判断PHY物理上未识别到网线),请TI的工程师帮忙分析下我们的问题可能出现在哪,是否和软件的BOOT有关系?(备注:3块单板均出现此问题,同时ET1011C芯片更换过)