OMAP137通过SPI接口连接了一个Flash,Flash烧进去程序之后实际的程序和编写的程序对不上,请问这是怎么回事,造成这种情况有哪些原因?
烧写的文件格式分别是AIX和HEX文件.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
OMAP137通过SPI接口连接了一个Flash,Flash烧进去程序之后实际的程序和编写的程序对不上,请问这是怎么回事,造成这种情况有哪些原因?
烧写的文件格式分别是AIX和HEX文件.
你好,
请教omap137的引导过程,我看了一些资料,也没找到比较全面系统的。如果有请麻烦给个链接
我下载了一个软件

我这样操作可以吗?
使用这个软件, 将我用dsp生成的应用程序*.out文件转化成*.bin文件,然后通过omap137的spi口烧到flash里,flash用25w64。
AISgen for D800K005这个软件中的那些选项都需要设置吗?这些选项在我们的应用程序的初始化中都有。
Dsp烧写25w64程序
Int16 spiflash_App( ) {
Int16 i, j;
Uint8* p8;
FILE *fPtr;
Uint32 *ptr;
Int32 fileSize = 0;
Int32 no_of_pages;
Int32 no_of_sectors;
Uint16 page_size;
spiflash_init(); // Initialize the SPI interface
if((fPtr = fopen("D:\\rmb_2cis1.bin","rb")) == NULL)
printf("UBL Open Failed.");
fileSize = ftell(fPtr);
page_size=256;
no_of_pages = fileSize/page_size + ((fileSize % page_size) ? 1 : 0);
spiflash_erase( 0, no_of_pages * spiflash_PAGESIZE); // Erase
i=0;
while(!feof(fPtr))
{
p8 = (Uint8*) tx;
if(!feof(fPtr)) {
fread(p8, 1, page_size, fPtr);
}
spiflash_write( ( Uint32 )tx, i * spiflash_PAGESIZE, spiflash_PAGESIZE );
printf("Writing APP at page offset: %d, number of pages: %d\n", i, no_of_pages);
i++;
}