请教TI工程师几个问题,麻烦帮忙解答一下,谢谢!
需求要求使用AM335X处理器且支持Nandflash(8-Bit)、EMMC、SD卡启动。
1、将SD卡挂在MMC0接口,将EMMC(8-Bit data)挂在MMC1接口上,按照文档要求,MMC仅支持4-Bit启动,请问用8-Bit EMMC,在启动的时候采用4-Bit Boot,启动后EMMC采用8-Bit是否可行?
2、由于EMMC占用了GPMC数据总线的低8位,将Nandflash挂在GPMC数据总线的高8位是否可行?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是的,如果是使用mmc1启动,需要按照TRM手册要求的配置方式,进行mmc1的设计。需要用AD0~D3
BBB的原理图可以参考:http://elinux.org/Beagleboard:BeagleBoneBlack#Hardware_Files
Table 26-29. Pins Used for MMC1 Boot
Signal name Pin Used in Device
clk gpmc_csn1
cmd gpmc_csn2
dat0 gpmc_ad0
dat1 gpmc_ad1
dat2 gpmc_ad2
dat3 gpmc_ad3