This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

8168 U-BOOT



你好:

   我在设置了BOOTCMD。我的ENVE的参数是

bootdelay=3
baudrate=115200
autoload=no
verify=yes
bootfile=uImage
ramdisk_file=ramdisk.gz
loadaddr=0x81000000
script_addr=0x80900000
loadbootscript=fatload mmc 0 ${script_addr} boot.scr
loaduimage=fatload mmc 0 ${loadaddr} uImage
bootscript= echo Running bootscript from MMC/SD to set the ENV...; source ${script_addr}
nandboot=echo Booting from nand ...; nandecc hw 0;run nandargs; nand read ${loadaddr} 280000 440000; bootm ${loadaddr}
updatesys=nand erase;mmc rescan 0;fatload mmc 0 0x81000000 u-boot.noxip.bin;nandecc hw 2;nand write.i 0x81000000 0x0 0x1c0000;nandecc hw 0;fatload mmc 0 0x81000000 uImage;nand write 0x81000000 0x280000  0x440000;fatload mmc 0 81000000 ubi.img;nandecc sw;nand write.i 81000000 6c0000 ${filesize};echo OK

updateuboot=mmc rescan 0;nand erase 0 1c0000;nandecc hw 2;fatload mmc 0 0x81000000 u-boot.noxip.bin;nand write.i 0x81000000 0x0 0x1c0000;nandecc hw 0;nand erase 280000 440000;fatload mmc 0 0x81000000 uImage;nand write 0x81000000 0x280000  0x440000;
ethaddr=d0:ff:50:b8:81:94
ethact=DaVinci EMAC
serverip=192.168.7.251
ipaddr=192.168.40.223
nandargs=setenv bootargs console=ttyO2,115200n8 notifyk.vpssm3_sva=0xBF900000 rootwait root=ubi0:rootfs ubi.mtd=3 rootfstype=ubifs rw mem=300M@0x80000000 mem=128M@0x9FC00000 vmalloc=500M earlyprink vram=70M ti816xfb.vram=0:16M,1:16M,2:6M ip=off noinitrd user_debug=31 init=/linuxrc ver=U-Boot 2010.06 (Sep 26 2014 - 04:10:22)
bootcmd=nand read 0x82000000 0x280000 0x300000;logo on 0x82000000 0xA0000000 100 60;nand read 0x81000000 0x00580000 0x260000;bootm 0x81000000
ver=U-Boot 2010.06 (Sep 29 2014 - 09:00:53)

然后我用SD卡启动出现

U-Boot 2010.06 (Jan 29 2013 - 09:37:35)

DRAM:  2 GiB
MMC:   OMAP SD/MMC: 0
Using default environment

Hit any key to stop autoboot:  0
raise: Signal # 8 caught
reading u-boot.bin

991732 bytes read
## Starting application at 0x80800000 ...


U-Boot 2010.06 (Sep 29 2014 - 09:00:53)

TI8168-GP rev 2.1

ARM clk: 1382MHz
DDR clk: 796MHz

I2C:   ready
DRAM:  2 GiB
NAND:  HW ECC BCH8 Selected
1024 MiB
MMC:   OMAP SD/MMC: 0

接着一直打印

ECC: uncorrectable

很长一段后直接进入U-BOOT命令行,不可以加载内核和文件系统这个问题怎么解决,谢谢。我用的是EZSDK的代码。