您好!
我司正为项目选型,有如下要求:
1)ARM9 及以上32位芯片,cpu主频400MHz以上,RAM和flash尽量大,完全可用于工业环境,性能稳定可靠;
2)带IIC、SPI、CAN、Tcp/Ip,多uart,USB2.0等接口且可扩展;
3)带LCD控制器且支持触摸屏;
4)支持嵌入式Linux软件系统;
请专家达人们推荐推荐!
致谢!
深圳金宏威
陈杰
1360 3090 921
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.