我现在采用DM6437芯片开发图像应用,程序在INT0中断中获取一帧图像并缓存到队列中,
请问是不是可以设置DM6437,修改进入INT0中断函数的频率啊,因为我发现现在获取图像的
速率达不到实时性的要求。如果可以设置,应该设置哪个寄存器?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
你是指的VDINT0么?如果是,中断频率是不能改变的。
你现在采集的是720x480 30f/s?如果不是,是多大分辨率每秒多少帧?
你好,
首先你需要找到是哪里的处理大于40ms,影响了实时性。请问你的算法处理每帧数据需要多少时间?如果处理时间是大于40ms的,那你的系统就无法做到实时。
VDINT的频率是和外部输入信号的VD频率一致的。