This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GPMC总线引脚配置未生效



以下是我的引脚配置和初始化函数:

static struct resource am335x_gpmc_resource[] = {
[0] = {
.start = 0x50000000,
.end = 0x50FFFFFF,
.flags = IORESOURCE_MEM
},
};

static struct platform_device am335x_gpmc_device = {
.name = "am335x_gpmc",
.id = 1,
.resource = am335x_gpmc_resource,
.num_resources = ARRAY_SIZE(am335x_gpmc_resource),
};
// module pin mux for gpmc
static struct pinmux_config gpmc_pin_mux[]={
{"gpmc_a1.gpmc_a1", OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA},
{"gpmc_a2.gpmc_a2", OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA},
{"gpmc_a3.gpmc_a3", OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA},
{"gpmc_a4.gpmc_a4", OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA},
{"gpmc_a5.gpmc_a5", OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA},
{"gpmc_a6.gpmc_a6", OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA},
{"gpmc_a7.gpmc_a7", OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA},
{"gpmc_a8.gpmc_a8", OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA},


{"gpmc_ad0.gpmc_ad0", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad1.gpmc_ad1", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad2.gpmc_ad2", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad3.gpmc_ad3", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad4.gpmc_ad4", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad5.gpmc_ad5", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad6.gpmc_ad6", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad7.gpmc_ad7", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad8.gpmc_ad8", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad9.gpmc_ad9", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad10.gpmc_ad10", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad11.gpmc_ad11", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad12.gpmc_ad12", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad13.gpmc_ad13", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad14.gpmc_ad14", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad15.gpmc_ad15", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},


{"gpmc_advn_ale.gpmc_advn_ale", OMAP_MUX_MODE0 | AM33XX_PULL_DISA},

{"gpmc_oen_ren.gpmc_oen_ren", OMAP_MUX_MODE0 | AM33XX_PULL_DISA},
{"gpmc_wen.gpmc_wen", OMAP_MUX_MODE0 | AM33XX_PULL_DISA},

{"gpmc_ben0_cle.gpmc_ben0_cle", OMAP_MUX_MODE0 | AM33XX_PULL_DISA},
{"gpmc_wpn.gpmc_wpn", OMAP_MUX_MODE7 | AM33XX_PIN_INPUT_PULLUP},

{"gpmc_clk.gpmc_wait1", OMAP_MUX_MODE2 | AM33XX_PIN_INPUT_PULLUP},
//{"gpmc_clk.gpmc_clk", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},

/*must be set as an input*/
{"gpmc_csn1.gpmc_clk", OMAP_MUX_MODE1 | AM33XX_PIN_INPUT_PULLUP},
//{"gpmc_csn1.gpmc_csn1", OMAP_MUX_MODE0 | AM33XX_PULL_DISA},


//{"gpmc_csn2.gpmc_csn2", OMAP_MUX_MODE0 | AM33XX_PULL_DISA},
{"gpmc_csn3.gpmc_csn3", OMAP_MUX_MODE0 | AM33XX_PULL_DISA},

{NULL, 0},
};

static void am335x_gpmc_init(void)
{
setup_pin_mux(gpmc_pin_mux);
platform_device_register(&am335x_gpmc_device);
}

最后在函数:static void __init am335x_evm_init(void)中添加了am335x_gpmc_init();

我在引脚初始化的时候将gpmc_csn1引脚作为同步时钟,所以设置为模式1.但是将编译后的内核烧写进开发板用devmem2打印出来的引脚配置却是模式7。

求解答

多谢!!!