This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: 无法使用主域can4

Part Number: TDA4VM

SDK:ti-processor-sdk-rtos-j721e-evm-08_01_00_13

在调试主域CAN4时,无法接收通过canoe接收can数据帧。MCAN4_TX、MCAN4_RX引脚配置没有问题。

当我通过MCAN4发送数据帧给canoe时,读取mcan4的状态位bus_off状态,并且触发了bus_off中断。

当我通过MCAN4接收canoe发送的数据时,无法收到数据,无法进入中断,此时读取MCAN4的状态为active.

读取状态的函数为:MCAN_getProtocolStatus。

请问以下,如何设置当can处于bus_off时,让其自动bus_on,这个需要调用哪一个api ?
并且希望TI工程师帮忙分析一下以上问题。谢谢。