我們的板子,開機log如下
從上電到login約需15sec
我們的功能僅用到gpmc for FPGA,1組ethernet,1組usb,其他都gpio
1.請問該如何加快開機時間呢??
2.我知道使用ramdisk 會拖慢開機時間,因生產問題,這沒辦法修改
3.我使用arago-base-tisdk-image-am335x-evm來做rootfs,並製作成ramdisk
lib與/usr/lib 哪些東西可以移去??
4.為什麼 Starting udev要花費將近3秒的時間呢??
U-Boot SPL 2013.01.01 (Oct 13 2014 - 14:58:52)
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
OMAP SD/MMC: 0
reading u-boot.img
reading u-boot.img
U-Boot 2013.01.01 (Oct 13 2014 - 14:58:52)
I2C: ready
DRAM: 256 MiB
WARNING: Caches not enabled
NAND: No NAND device found!!!
0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - readenv() failed, using default environment
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw, usb_ether
Hit any key to stop autoboot: 0
mmc0 is current device
SD/MMC found on device 0
reading uEnv.txt
196 bytes read in 4 ms (47.9 KiB/s)
Loaded environment from uEnv.txt
Importing environment from mmc ...
Running uenvcmd ...
reading uImage
2653960 bytes read in 252 ms (10 MiB/s)
reading ramdisk.gz
15953390 bytes read in 1499 ms (10.1 MiB/s)
## Booting kernel from Legacy Image at 80200000 ...
Image Name: Linux-3.2.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2653896 Bytes = 2.5 MiB
Load Address: 80008000
Entry Point: 80008000
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.2.0 (root@am335xhost) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #2 Tue Oct 7 12:35:32 CST 2014
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES2.1 (neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/ram0 rw rootfstype=ext2 initrd=0x81000000,64M
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 256MB = 256MB total
[ 0.000000] Memory: 188868k/188868k available, 73276k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0497000 (4668 kB)
[ 0.000000] .init : 0xc0497000 - 0xc04ce000 ( 220 kB)
[ 0.000000] .data : 0xc04ce000 - 0xc0525860 ( 351 kB)
[ 0.000000] .bss : 0xc0525884 - 0xc0552e64 ( 182 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[ 0.000000] omap_dm_timer_switch_src: Switching to HW default clocksource(sys_clkin_ck) for timer1, this may impact timekeeping in low power state
[ 0.000000] OMAP clocksource: GPTIMER1 at 24000000 Hz
[ 0.000000] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000164] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[ 0.087769] pid_max: default: 32768 minimum: 301
[ 0.087863] Security Framework initialized
[ 0.087948] Mount-cache hash table entries: 512
[ 0.088270] CPU: Testing write buffer coherency: ok
[ 0.107651] omap_hwmod: gfx: failed to hardreset
[ 0.123423] omap_hwmod: pruss: failed to hardreset
[ 0.124381] print_constraints: dummy:
[ 0.124677] NET: Registered protocol family 16
[ 0.126387] OMAP GPIO hardware version 0.1
[ 0.128193] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.129702] omap_i2c.1: alias fck already exists
[ 0.130947] edma.0: alias fck already exists
[ 0.130963] edma.0: alias fck already exists
[ 0.130977] edma.0: alias fck already exists
[ 0.145334] bio: create slab <bio-0> at 0
[ 0.147039] SCSI subsystem initialized
[ 0.147597] usbcore: registered new interface driver usbfs
[ 0.147865] usbcore: registered new interface driver hub
[ 0.148031] usbcore: registered new device driver usb
[ 0.148328] registerd cppi-dma Intr @ IRQ 17
[ 0.148340] Cppi41 Init Done Qmgr-base(d087a000) dma-base(d0878000)
[ 0.148347] Cppi41 Init Done
[ 0.148370] musb-ti81xx musb-ti81xx: musb0, board_mode=0x11, plat_mode=0x1
[ 0.148630] musb-ti81xx musb-ti81xx: musb1, board_mode=0x11, plat_mode=0x1
[ 0.149412] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[ 0.150943] tps65910 1-002d: JTAGREVNUM 0x0
[ 0.153208] print_constraints: VRTC:
[ 0.154572] print_constraints: VIO: at 1500 mV
[ 0.156781] print_constraints: VDD1: 600 <--> 1500 mV at 1325 mV normal
[ 0.158981] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal
[ 0.159911] print_constraints: VDD3: 5000 mV
[ 0.161241] print_constraints: VDIG1: at 1800 mV
[ 0.162590] print_constraints: VDIG2: at 1800 mV
[ 0.163924] print_constraints: VPLL: at 1800 mV
[ 0.165262] print_constraints: VDAC: at 1800 mV
[ 0.166613] print_constraints: VAUX1: at 1800 mV
[ 0.167970] print_constraints: VAUX2: at 3300 mV
[ 0.169311] print_constraints: VAUX33: at 3300 mV
[ 0.170649] print_constraints: VMMC: at 3300 mV
[ 0.171026] tps65910 1-002d: No interrupt support, no core IRQ
[ 0.172834] Switching to clocksource gp timer
[ 0.184455] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.184618] musb-hdrc musb-hdrc.0: dma type: dma-cppi41
[ 0.184877] MUSB0 controller's USBSS revision = 4ea20800
[ 0.184905] musb0: Enabled SW babble control
[ 0.185317] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 0.185400] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
[ 0.185525] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.185536] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.185547] usb usb1: Product: MUSB HDRC host driver
[ 0.185554] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd
[ 0.185562] usb usb1: SerialNumber: musb-hdrc.0
[ 0.186253] hub 1-0:1.0: USB hub found
[ 0.186280] hub 1-0:1.0: 1 port detected
[ 0.186702] musb-hdrc musb-hdrc.0: USB Host mode controller at d083c000 using DMA, IRQ 18
[ 0.186853] musb-hdrc musb-hdrc.1: dma type: dma-cppi41
[ 0.187110] MUSB1 controller's USBSS revision = 4ea20800
[ 0.187132] musb1: Enabled SW babble control
[ 0.187512] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.187549] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
[ 0.187632] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.187643] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.187653] usb usb2: Product: MUSB HDRC host driver
[ 0.187660] usb usb2: Manufacturer: Linux 3.2.0 musb-hcd
[ 0.187668] usb usb2: SerialNumber: musb-hdrc.1
[ 0.188237] hub 2-0:1.0: USB hub found
[ 0.188259] hub 2-0:1.0: 1 port detected
[ 0.188658] musb-hdrc musb-hdrc.1: USB Host mode controller at d083e800 using DMA, IRQ 19
[ 0.189022] NET: Registered protocol family 2
[ 0.189191] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.189438] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.189554] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.189623] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.189633] TCP reno registered
[ 0.189642] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.189659] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.189814] NET: Registered protocol family 1
[ 0.190031] RPC: Registered named UNIX socket transport module.
[ 0.190042] RPC: Registered udp transport module.
[ 0.190048] RPC: Registered tcp transport module.
[ 0.190054] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.190248] Trying to unpack rootfs image as initramfs...
[ 0.190939] rootfs image is not initramfs (no cpio magic); looks like an initrd
[ 0.487899] Freeing initrd memory: 65536K
[ 0.487921] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.498378] VFS: Disk quotas dquot_6.5.2
[ 0.498435] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.498874] msgmni has been set to 496
[ 0.501472] alg: No test for stdrng (krng)
[ 0.502042] io scheduler noop registered
[ 0.502052] io scheduler deadline registered
[ 0.502108] io scheduler cfq registered (default)
[ 0.502636] Could not set LED4 to fully on
[ 0.543768] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 1.265650] console [ttyO0] enabled
[ 1.269718] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 1.277444] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 1.285150] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 1.292829] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 1.300541] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 1.308607] omap4_rng omap4_rng: OMAP4 Random Number Generator ver. 2.00
[ 1.322564] brd: module loaded
[ 1.329472] loop: module loaded
[ 1.332949] i2c-core: driver [tsl2550] using legacy suspend method
[ 1.339409] i2c-core: driver [tsl2550] using legacy resume method
[ 1.345846] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.452863] No daughter card found
[ 1.456449] at24 1-0055: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.463736] The board is a AM335x Starter Kit.
[ 1.468559] omap_hsmmc.0: alias fck already exists
[ 1.474283] _omap_mux_get_by_name: Could not find signal gpmc_csn1.gpio1_29
[ 1.481570] _omap_mux_get_by_name: Could not find signal gpmc_csn2.gpio1_30
[ 1.488875] _omap_mux_get_by_name: Could not find signal gpmc_csn3.gpio1_31
[ 1.498474] registered am33xx_sr device
[ 1.503789] vcan: Virtual CAN interface driver
[ 1.508439] CAN device driver interface
[ 1.512443] CAN bus driver for Bosch D_CAN controller 1.0
[ 1.562892] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[ 1.569358] davinci_mdio davinci_mdio.0: detected phy mask fffffffe
[ 1.576783] phy read clk = 0x3def
[ 1.580486] phy read clk = 0x3ed6
[ 1.584452] phy read rxd = 0x7777
[ 1.588156] phy read rxd = 0x0
[ 1.591512] davinci_mdio.0: probed
[ 1.595079] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
[ 1.602719] usbcore: registered new interface driver zd1201
[ 1.608704] usbcore: registered new interface driver cdc_ether
[ 1.614936] usbcore: registered new interface driver cdc_eem
[ 1.620957] usbcore: registered new interface driver dm9601
[ 1.626826] cdc_ncm: 04-Aug-2011
[ 1.630315] usbcore: registered new interface driver cdc_ncm
[ 1.636242] Initializing USB Mass Storage driver...
[ 1.641519] usbcore: registered new interface driver usb-storage
[ 1.647808] USB Mass Storage support registered.
[ 1.652993] mousedev: PS/2 mouse device common for all mice
[ 1.659311] i2c /dev entries driver
[ 1.803647] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.811962] cpuidle: using governor ladder
[ 1.816649] cpuidle: using governor menu
[ 1.822839] omap4_aes_mod_init: loading AM33X AES driver
[ 1.828512] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02
[ 1.835191] omap4_aes_probe: probe() done
[ 1.839574] omap4_sham_mod_init: loading AM33X SHA/MD5 driver
[ 1.845709] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03
[ 1.860565] omap4_sham_probe: probe() done
[ 1.867262] oprofile: hardware counters not available
[ 1.872555] oprofile: using timer interrupt.
[ 1.877051] nf_conntrack version 0.5.0 (3975 buckets, 15900 max)
[ 1.883746] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 1.889398] TCP cubic registered
[ 1.892771] NET: Registered protocol family 17
[ 1.897448] can: controller area network core (rev 20090105 abi 8)
[ 1.903995] NET: Registered protocol family 29
[ 1.908639] can: raw protocol (rev 20090105)
[ 1.913110] can: broadcast manager protocol (rev 20090105 t)
[ 1.919058] Registering the dns_resolver key type
[ 1.924029] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 1.932043] ThumbEE CPU extension supported.
[ 1.936569] mux: Failed to setup hwmod io irq -22
[ 1.942057] Power Management for AM33XX family
[ 1.946908] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[ 1.953602] Copied the M3 firmware to UMEM
[ 1.957954] Cortex M3 Firmware Version = 0x181
[ 1.964275] create_regulator: VDD1: Failed to create debugfs directory
[ 1.972592] smartreflex smartreflex: am33xx_sr_probe: Driver initialized
[ 1.985425] clock: disabling unused clocks to save power
[ 2.000223] Detected MACID=1c:ba:8c:b7:53:1c
[ 2.005714] cpsw: Detected MACID = 1c:ba:8c:b7:53:1e
[ 2.012155] RAMDISK: gzip image found at block 0
[ 2.042440] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 2.063042] mmc0: new high speed SD card at address e624
[ 2.083084] mmcblk0: mmc0:e624 SU02G 1.84 GiB
[ 2.093819] mmcblk0: p1
[ 3.733836] VFS: Mounted root (ext2 filesystem) on device 1:0.
[ 3.740275] Freeing init memory: 220K
INIT: version 2.88 booting
Error opening /dev/fb0: No such device
Starting udev
Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory
bootlogd.
ALSA: Restoring mixer settings...
/usr/sbin/alsactl: load_state:1686: No soundcards found...
Configuring network interfaces... done.
hwclock: can't open '/dev/misc/rtc': No such file or directory
Tue Jun 25 23:08:00 UTC 2013
hwclock: can't open '/dev/misc/rtc': No such file or directory
Configuring update-modules.
INIT: Entering runlevel: 5
[ 6.532921] phy read clk = 0x3ed6
[ 6.536606] phy read clk = 0x3ed6
[ 6.540571] phy read rxd = 0x0
[ 6.544016] phy read rxd = 0x0
[ 6.547474] net eth0: CPSW phy found : id is : 0x221622
[ 6.566315] Disabling lock debugging due to kernel taint
dbus.
Starting telnet daemon.
hwclock: can't open '/dev/misc/rtc': No such file or directory
Starting syslogd/klogd: done
Stopping Bootlog daemon: bootlogd.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am335x-evm ttyO0
Arago 2013.05 am335x-evm ttyO0
am335x-evm login: