新买的板子,第一次上电时应该是led1和led2最后都亮的吧,目前我的LED1不亮是不是说明RAM TEST没通过?这种情况下应该怎么办呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
新买的板子,第一次上电时应该是led1和led2最后都亮的吧,目前我的LED1不亮是不是说明RAM TEST没通过?这种情况下应该怎么办呢?
Andy Yin1 说:上电后,mezzanine emulator子卡上的D3先亮,Emulator boot起来之后D3两边的D1与D2亮,这个过程需要一段时间,可以稍等片刻。reset full不会擦除flash及EEPROM上烧写的数据。
mezzanine emulator是指上面那个仿真器XDS560V2么,我的板子是LE,测试说明上是指6678L的,正常情况下是下面板卡的LED1和LED2亮,我的目前经过一段时间后只有LED1亮,但是仿真器上的D1,D2,D3情况跟您说的是一致的,是不是说明没问题呢?
另外,是否可以将XDS560V2从板卡下卸下来,因为quick start guide里好像都是按照6678L的讲解?