This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ti内核编译后启动不了



U-Boot# fatload mmc 0 0x82000000 uImage
reading uImage
3342536 bytes read in 679 ms (4.7 MiB/s)
U-Boot# bootm 0x82000000
## Booting kernel from Legacy Image at 82000000 ...
Image Name: Linux-3.2.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3342472 Bytes = 3.2 MiB
Load Address: 00008000
Entry Point: 00008000
Verifying Checksum ... OK
Loading Kernel Image ... data abort

MAYBE you should read doc/README.arm-unaligned-accesses

pc : [<9ff9fd84>] lr : [<9ff76374>]
sp : 9fe53d98 ip : 00000000 fp : 9fe57544
r10: 00000000 r9 : 9fe53f38 r8 : 82000000
r7 : 9ffb7bfc r6 : 00000000 r5 : 00000000 r4 : 00008000
r3 : 00000000 r2 : 00330087 r1 : 82000040 r0 : 00008000
Flags: nzCv IRQs off FIQs on Mode SVC_32
Resetting CPU ...

这是什么原因???