This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678 MCSDK中的IBL source有人用过吗?串口不能输出信息



您好,

首先我在CCS下用platform_test工程对串口进行测试,可以在PC中断收发信息。

然后我将MCSDK中的IBL源文件进行编译,将生成的i2crom_0x51_c6678_le.bin,i2cparam_0x51_c6678_le_0x500.out,i2cConfig.gel三个文件按照要求烧到EEPROM中,将DSP启动模式设置为I2C。

结果dsp通过I2C启动,串口并没有信息输出。

我对比了IBL里面UART_INIT()函数和CCS工程里面的UART_INIT()函数,发现初始化参数不同,然后将IBL里面的初始化参数改成CCS工程里面的参数,结果串口仍然不输出信息。

有人直接用过MCSDK中的IBL源文件吗?搞了好多天了。。。求帮助