我想问下DM8168的USB 是个非完整功能的OTG,只能设置为主或从,我手头的板上USB是为主模式,现在我想把DM8168做为从端,那board代码中USB模式应该是CONFIG_USB_MUSB_OTG还是CONFIG_USB_GADGET_MUSB_HDRC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想问下DM8168的USB 是个非完整功能的OTG,只能设置为主或从,我手头的板上USB是为主模式,现在我想把DM8168做为从端,那board代码中USB模式应该是CONFIG_USB_MUSB_OTG还是CONFIG_USB_GADGET_MUSB_HDRC?
你好,
你使用的是PG2.x的DM8168么?如果是,应该由外部USB_ID的状态来决定是host还是slave,所以我觉得应该是配置OTG。其他配置,请参考链接:http://processors.wiki.ti.com/index.php/TI81XX_PSP_USB_Driver_User_Guide#USB_Device_Configuration。
您好!不清楚用的是PG1.x还是PG2.x的,在IC的表面丝印上可以直接识别吗?我使用的DM8168丝印有型号是DM8168BCYG 32A2R8W,右上角有个“2”,左下角有字符“ G1”,G1下面有三个字符“CYG”。
你好,
你使用的芯片是PG2.0的。参考勘误表的信息你可以从丝印上了解芯片的版本号。请到TI网站上下载勘误表:
http://www.ti.com/product/tms320dm8168
TMS320DM816x DaVinci Video Processors Silicon Errata (Rev. 2.1, 2.0, 1.1, & 1.0) (Rev. E)
可是dm8168的Pin中好像找不到ID pad,是否只能以软件方式设置iddlg?
DM8168没有USB ID脚,所以是通过软件方式配置,而且不支持OTG.
http://processors.wiki.ti.com/index.php/DM81xx_AM38XX_USB_User_Guide