This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm8127使用DSKT2_createAlg()创建句柄失败



    pObj->algHndl = DSKT2_createAlg((Int)scratchId,
            (IALG_Fxns *)algFxns, NULL,(IALG_Params *)&prm);
    Vps_rprintf(" IVD_open pObj->algHndl %x !!!\n",pObj->algHndl);

。。。。。。。。。

#define IALGFXNS  \
    &IVD_TI_IALG,  /* module ID */                         \
    NULL,            /* activate */                          \
    IVD_TI_alloc,  /* alloc */                             \
    NULL,            /* control (NULL => no control ops) */  \
    NULL,            /* deactivate */                        \
    IVD_TI_free,   /* free */                              \
    IVD_TI_initObj,/* init */                              \
    NULL,            /* moved */                             \
    IVD_TI_numAlloc             /* numAlloc (NULL => IALG_MAXMEMRECS) */

  IVD_TI_numAlloc ()运行通过,IVD_TI_alloc()运行时不通过,IVD_TI_initObj没有运行

Int IVD_TI_alloc(const IALG_Params *algParams, IALG_Fxns **pf, IALG_MemRec memTab[])
{
 XDAS_Int32  uRegin_width;
 XDAS_Int32  uRegin_height;
  // XDAS_Int32 i;
 XDAS_Int32  size;

 const IVD_Params *params = (IVD_Params *)algParams;
 Vps_rprintf("IVD_TI_alloc maxWidth %d, maxHeight %d ,size %d!!!\n",params->maxWidth,params->maxHeight,params->size);

  /* Request memory for my object */
  memTab[0].size = sizeof(IVD_TI_Obj);
  memTab[0].alignment = 0;
  memTab[0].space = IALG_DARAM0;
//  memTab[0].space = IALG_EXTERNAL;
  memTab[0].attrs = IALG_PERSIST;

 Vps_rprintf("IVD_TI_alloc memTab[0] size %d  base:0x%x!!!\n",memTab[0].size,memTab[0].base);

  /* Request memory */
  memTab[1].size = sizeof(ALGCFGS);
  memTab[1].alignment = 0;
  memTab[1].space = IALG_DARAM0; //mod by david 20130513
//  memTab[1].space = IALG_EXTERNAL;
  memTab[1].attrs = IALG_PERSIST;

 Vps_rprintf("IVD_TI_alloc memTab[1] size %d  base:0x%x!!!\n",memTab[1].size,memTab[1].base);
  /* Request memory*/
  memTab[2].size = sizeof(ALGPARAMS);
  memTab[2].alignment = 0;
  //memTab[2].space = IALG_DARAM0; //mod by david 20130513
  memTab[2].space = IALG_EXTERNAL;
  memTab[2].attrs = IALG_SCRATCH;  //
   Vps_rprintf("IVD_TI_alloc memTab[2] size %d  base:0x%x!!!\n",memTab[2].size,memTab[2].base);
  /* Request memory*/
  size = 0;
  uRegin_width = DETECTRECT_WIDTH_MAX1;
  uRegin_height = DETECTRECT_HEIGHT_MAX;
  //size = uRegin_width*uRegin_height*5;   //每个speed检测器有五个大小相同的buf
 // size = uRegin_width*uRegin_height*7;   //每个speed检测器有6个大小相同的buf, mod by david 20130826 for ivd2.0
  size = uRegin_width*uRegin_height*10;                                           //20140706  增加4个  queue
  memTab[3].size = size;    //可变大小,由下载配置项决定
  memTab[3].alignment = 0;
  //memTab[3].space = IALG_DARAM0;   //暂时使用外存
  memTab[3].space = IALG_EXTERNAL; //暂时使用外存
  memTab[3].attrs = IALG_SCRATCH;


  /* Request memory */
  size = DETECTRECT_WIDTH_MAX1 * DETECTRECT_HEIGHT_MAX * sizeof(Uint32); //按最大区域设置

  ///全部default为最大
  // size = sizeof(CAMERA_STRUCT) + \
    // sizeof(LANE_STRUCT_DEF)*MAX_LANE + \
    // uLaneAmount * sizeof(SPEED_DETECT_STRUCT) + \
    // size;
  size = sizeof(CAMERA_STRUCT) + \
    sizeof(LANE_STRUCT_DEF)*MAX_LANE + \
    MAX_LANE * sizeof(SPEED_DETECT_STRUCT) + \
    size;
  memTab[4].size = size;
  memTab[4].alignment = 0;
  memTab[4].space = IALG_EXTERNAL;
  memTab[4].attrs = IALG_PERSIST;

  /* Request memory */
  size = 0;
  uRegin_width = DETECTRECT_WIDTH_MAX1;////768
  uRegin_height = DETECTRECT_HEIGHT_MAX;
  //size = uRegin_width*uRegin_height*5;
 // size = uRegin_width*uRegin_height*6;  

  size = uRegin_width*uRegin_height*10;   ////20140706 add 4 memory quene  按照最大的768×576 分配
  memTab[5].size = size;
  memTab[5].alignment = 0;
  memTab[5].space = IALG_EXTERNAL;
  memTab[5].attrs = IALG_PERSIST;

  /* Request memory */ //added by david 20130903 for ivd2.0
  size = 0;
  size = 200*300* sizeof(CPoint);  ////20140706

  memTab[6].size = size;
  memTab[6].alignment = 0;
  memTab[6].space = IALG_EXTERNAL;
  memTab[6].attrs = IALG_PERSIST;

  /* Request memory */ //2014
  size = 0;
  size = 1 * sizeof(CForeground_Array);

  memTab[7].size = size;
  memTab[7].alignment = 0;
  memTab[7].space = IALG_EXTERNAL;
  memTab[7].attrs = IALG_PERSIST;
////20140708
  size = 0;
  size = uRegin_width *uRegin_height* sizeof(unsigned char);  ////20140706

  memTab[8].size = size;
  memTab[8].alignment = 0;
  memTab[8].space = IALG_EXTERNAL;
  memTab[8].attrs = IALG_PERSIST;

  Vps_rprintf("IVD_TI_alloc memTab[8] size %d  base:0x%x!!!\n",memTab[8].size,memTab[8].base);
    return (MTAB_NRECS);
}

打印信息:

 [c6xdsp ] IVD_open maxWidth 320, maxHeight 192 !!!
 [c6xdsp ]  IVD_TI_numAlloc MTAB_NRECS:9 !!!
 [c6xdsp ] IVD_TI_alloc maxWidth 320, maxHeight 192 ,size 12!!!
 [c6xdsp ] IVD_TI_alloc memTab[0] size 312  base:0x0!!!
 [c6xdsp ] IVD_TI_alloc memTab[1] size 7056  base:0x0!!!
 [c6xdsp ] IVD_TI_alloc memTab[2] size 1872  base:0x0!!!
 [c6xdsp ] IVD_TI_alloc memTab[8] size 442368  base:0x0!!!

 [host] FUN: [MultiCh_createTriStreamFullFtr] LINE: 1127
 [c6xdsp ]  IVD_open pObj->algHndl 0 !!!
 [m3vpss ] FUN: System_linkGetInfo LINE: 86
 [m3vpss ] FUN: System_linkGetInfo LINE: 97
 [m3vpss ]  13141: FD   : Alg Create Done !!!
 [c6xdsp ]  Creat DSKT2_createAlg failed !!!为什么分配不成功?需要配置什么文件吗