This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DM368运行encodec时,会出错:
rsz_set_output_address 0
rsz_set_output_address 1
Unable to handle kernel NULL pointer dereference at virtual address 00000003
pgd = c26d8000
[00000003] *pgd=822b9031
, *pte=00000000, *ppte=00000000
我们自己做的dm368板子,encode运行几分钟后会出错
谁遇到过?
你好我也在搞dm368,我想问你下,那个uboot配置参数是用什么,比如:
setenv bootargs mem=60M console=ttyS0,115200n8 noinitrd rw ip=192.168.1.80:255.255.255.0:192.168.1.1 root=/dev/nfs nfsroot=192.168.1.100:/home/davinci/dm368/dvsdk_dm368_4_02_00_06/filesystem/dm368rootfs video=davincifb:osd0=720x576x16,4050K dm365_imp.oper_mode=0 davinci_capture.device_type=4
你用的是什么?谢谢
setenv bootargs console=ttyS0,115200n8 rw dm365_imp.oper_mode=0 video=davincifb:vid0=OFF:vid1=OFF:osd0=480x272x16,4050K mem=48MB davinci_capture.device_type=4 vpfe_capture.cont_bufsize=12582912 davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=PAL root=/dev/nfs nfsroot=192.168.10.231:/root/targetfs ip=192.168.10.203:192.168.10.231:192.168.10.1:255.255.255.0::eth0:off
我后来用UBL_DM36x_NAND.bin启动板子,就是把ARM、DSP等频率降下来,ARM跑297Mhz,encode就能稳定运行一天多。
估计硬件布板可能有问题,我还要进一步测试。