This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6678 pdsp



您好!

            我想这样使用6678的pdsp1,用于多核导航器的消息机制中,具体如下:

            8个核分别配置pdsp1,这样相应核上产生中断时,我想要pdsp1分别将描述符的地址搬到之前配置

      好的各核独立的list address中。比如我想要pdsp1监视50事件的720到727队列,720队列上来了一个描述符,

      pdsp1则将描述符的地址搬到地址1。721队列来了一个描述符,pdsp1则将描述符的地址搬到地址2等等。

           不知能否行的通,怎么实现?

           谢谢!

  • 可以,可以分别使用多个channel,也可以使用一个channel同时监视多个queue,参考navigator user guide及STK navigator例程。

    STK: http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/t/47664.aspx