This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于给5535开发板导入程序的问题

Other Parts Discussed in Thread: TIDM-LPBP-TCHMP3PLAYER, TMS320C5535

1.我买了一块5535的开发板,对两个USB接口的功能不是太了解。J1是miniUSB接口,是直接和5535芯片相连的,我用J1和电脑连接,装好驱动后电脑的声音可以听到,他是否还有其他功能呢,比如给开发板导入程序?

2.我对软件部分一窍不通,我用J2接口和电脑连接,打开CCS,可以在开发板上运行流水灯的程序。请问,给开发板导入程序以后,如何才能保存到开发板上,让开发板供电以后,就可以直接运行已经灌入开发板的程序?

3.我看到了一个基于5535芯片做的MP3,www.ti.com.cn/.../tidm-lpbp-tchmp3player,

这个MP3上的JTAG接口直接和仿真器相连的是否是12345这5个引脚,我是否可以用USB上的5个引脚,来代替JTAG这5个引脚和仿真器相连。因为我看到5535开发板上仿真芯片部分,EMU0和EMU1两个引脚是空的。

  • 1. 请问你用的c5535开发板的具体型号是什么?miniUSB什么功能可以通过相应的原理图查看。

    2. 看开发板上有没有Flash或者EEPROM可以保存程序,C5535器件本身不能保存代码。

    3. 我看了一下这块MP3板子的原理图,并没有设计JTAG接口,所以不支持JTAG调试。

  • 1,我用的板子是这个http://www.ti.com.cn/tool/cn/TMDX5535EZDSP?keyMatch=5535&tisearch=Search-CN,我不太懂这个迷你USB是做什么用的。

    这是5535芯片的介绍,我不太懂,这些RAM不能保存程序吗

    3.那个MP3板子没有焊接JTAG接口,只是在板子上留了位置,我在想,我如果重新设计一个,能否把jtag接口用USB接口代替,因为JTAG接口真正和仿真器相连是有5个引脚,USB也有5个引脚,我只是想换个接口,是否能实现

  • 您好,请教一下,我买的是TMS320C5535 eZdsp ,我遇到一个问题,“

    Error connecting to the target:
    (Error -151 @ 0x0)
    This utility failed to open the adapter for a custom emulator.
    The adapter returned an error.
    (Release 5.0.429.0)

    之前请教了,说教我升级软件,我现在的软件是Code Composer Studio v4,还是不行,我现在和电脑连接的是J1,然后出现的这个问题,我想请问一下,我这个问题是“J1”和“J2”连接问题还是其他什么问题?还有“J1”,“J2”的区别是什么地方?谢谢您的解答。

  • 如果想让CCS平台和开发板相连接,必须用J2口连接电脑,然后按照开发板上CCS的指南,一步一步操作就能连上了,V4版本的可以用。我用J1口连接的时候,开始没有打开CCS软件,开发板找不到驱动,等我打开了CCS以后,开发板就可以找到驱动了,我也想不明白为什么装驱动还要打开CCS。J1口连接电脑了以后,我只能用来听电脑上的声音,只能证明我的驱动是装好了,其他功能,比如写程序什么的,就不知道行不行了,我也在请教TI的员工,到底这个J1口有没有其他的功能。

  • 还请教一个问题可以吗?下载程序,调试是连接J2口吗?谢谢

  • 接J2口是对的。

    为什么TI员工不来回答问题了,我的问题还没人给解决啊

  • 我也想问,你好 我是刚开始学DSP的,请你多多指教!!!

  • wang john 说:

    1,我用的板子是这个http://www.ti.com.cn/tool/cn/TMDX5535EZDSP?keyMatch=5535&tisearch=Search-CN,我不太懂这个迷你USB是做什么用的。

    这是5535芯片的介绍,我不太懂,这些RAM不能保存程序吗

    3.那个MP3板子没有焊接JTAG接口,只是在板子上留了位置,我在想,我如果重新设计一个,能否把jtag接口用USB接口代替,因为JTAG接口真正和仿真器相连是有5个引脚,USB也有5个引脚,我只是想换个接口,是否能实现



    1.  J1就是一般的miniusb口,不具备JTAG调试功能,主要是用在跑audio demo例程时,ezdsp作为一个usb headset.

    2. RAM不是非易失性memory, 掉电后内容不会保存。

    3. JTAG口和USB口的协议不一样,不能把JTAG口直接接usb口。

  • guangsheng zheng 说:

    您好,请教一下,我买的是TMS320C5535 eZdsp ,我遇到一个问题,“

    Error connecting to the target:
    (Error -151 @ 0x0)
    This utility failed to open the adapter for a custom emulator.
    The adapter returned an error.
    (Release 5.0.429.0)

    之前请教了,说教我升级软件,我现在的软件是Code Composer Studio v4,还是不行,我现在和电脑连接的是J1,然后出现的这个问题,我想请问一下,我这个问题是“J1”和“J2”连接问题还是其他什么问题?还有“J1”,“J2”的区别是什么地方?谢谢您的解答。



    J1没有debug功能,是普通的miniusb口,跑audio demo例程时作为usb通信口。

    J2是板上内嵌仿真口,可以不用外接仿真器,直接通过usb口和PC相连进行代码调试。

    所以你要用J2口。

  • wang john 说:

    如果想让CCS平台和开发板相连接,必须用J2口连接电脑,然后按照开发板上CCS的指南,一步一步操作就能连上了��V4版本的可以用。我用J1口连接的时候,开始没有打开CCS软件,开发板找不到驱动,等我打开了CCS以后,开发板就可以找到驱动了,我也想不明白为什么装驱动还要打开CCS。J1口连接电脑了以后,我只能用来听电脑上的声音,只能证明我的驱动是装好了,其他功能,比如写程序什么的,就不知道行不行了,我也在请教TI的员工,到底这个J1口有没有其他的功能。

    这是因为跑了audio demo 程序,可以看一下QSG.
    http://support.spectrumdigital.com/boards/ezdsp5535/revc/files/EZDSP5535_QuickStartGuide.pdf

  • guangsheng zheng 说:

    还请教一个问题可以吗?下载程序,调试是连接J2口吗?谢谢



    是的,用J2口,可以先看一下下面5535开发板的文档,有各个功能模块的介绍和原理图。
    http://support.spectrumdigital.com/boards/ezdsp5535/revc/files/ezdsp5535_TechRef_RevC.pdf

  • 建议有问题,另起新贴啊,方便其他客户查看。

  • 请问,5535上128K的rom是可以存储程序的吧,是否是上电自举,掉电后程序会丢掉吗

  • ROM是Read Only Memory只读memory, 用户是不能对其写的,只能读。

    要对ROM写,只有进行Mask掩膜,这个只能TI做,用户做不了。