This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678 SRIO



使用的是DSP TI C6670和C6678与SRIO( IDT1848)交换芯片连接,速率为5G,端口为port0:4X。 问题: 1.SRIO初始化完后,.DSP与交换芯片lane 同步时有时lane同步不上(有时为正常4 lane,有时为3个lane或者2个lane);请问是什么原因?

  • 检查一下两侧的收发信号眼图质量,可能眼图不好导致。

  • 你好,看到你也在用1848和6678的互联,想请教一下1848的配置问题

    我使用ARM通过I2C配置1848可以成功,两片6678可以进行正常通信。但是,想用6678发送维护包给1848进行配置时,发现ARM写进去的寄存器的值都可以通过维护包读到,但是没法让6678使用维护包进行更改1848的各个寄存器的值。也就是说6678只能读1848而不能写,请问你遇到这种问题了吗,是怎么解决的?进行维护包写1848的时候,需要一些额外的操作比如说打开1848的写开关之类的吗,谢谢!