This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IBL 二次Boot的多核启动及工具链问题



各位好:

    我现在在使用同事做的一个板子,板子上电时FPGA会将DSP设置为I2C IBL Boot,并初始化Boot参数表和DDR,普通单核任务的L2配置为0x00820000后,只需要将编译生成的.out文件改为.bin然后烧录到NOR Flash就可以正常运行。

    我现在有8个工程,分别对应一个core(通过参考帖子www.deyisupport.com/.../8065.aspx 已经能够通过帖子作者提供的工具链实现SPI Flash多核启动),请问是否有相关工具链(或修改前面那个帖子提供的工具链)能将8个.out文件转换为.dat文件并能够实现IBL二次Boot方式下的多核启动呢?有没有相关例子、文档可以参考?

    万分感谢!!!