This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好 , 我使用BBB SDK 2.0 eMMC 燒錄 後發現重開機一直只能夠停在下列的階段...重複開關機次都一樣...請問有甚麼方式解決或是清除可以讓我重新再燒錄?謝謝!
U-Boot SPL 2013.01.01 (Sep 01 2016 - 00:31:54)
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
有時候會會出現下列訊息 :
U-Boot SPL 2013.01.01 (Sep 01 2016 - 00:31:54)
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
Hi Jian工 您好~
請問我燒錄完後都會出現下列訊息,似乎是敘述空間不夠需要刪掉程序...等等
下列是Log & uniflash & debrick 內容 :
[eMMC 燒錄訊息] :
CCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCC
U-Boot SPL 2013.01.01 (Oct 21 2014 - 14:08:51)
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
Using default environment
usb_ether
using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in
MAC 1c:ba:8c:96:0d:6a
HOST MAC de:ad:be:af:00:00
RNDIS ready
musb-hdrc: peripheral reset irq lost!
high speed config #2: 2 mA, Ethernet Gadget, using RNDIS
USB RNDIS network up!
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
Using usb_ether device
TFTP from server 192.168.100.1; our IP address is 192.168.100.2
Filename 'u-boot-restore.img'.
Load address: 0x807fffc0
Loading: #########################
873 KiB/s
done
Bytes transferred = 365104 (59230 hex)
U-Boot 2013.01.01 (Oct 21 2014 - 14:08:51)
I2C: ready
DRAM: 512 MiB
WARNING: Caches not enabled
NAND: No NAND device found!!!
0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - readenv() failed, using default environment
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw, usb_ether
Hit any key to stop autoboot: 0
using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in
MAC 1c:ba:8c:96:0d:6a
HOST MAC de:ad:be:af:00:00
RNDIS ready
musb-hdrc: peripheral reset irq lost!
high speed config #2: 2 mA, Ethernet Gadget, using RNDIS
USB RNDIS network up!
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
DHCP client bound to address 192.168.100.2
using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in
MAC 1c:ba:8c:96:0d:6a
HOST MAC de:ad:be:af:00:00
RNDIS ready
high speed config #2: 2 mA, Ethernet Gadget, using RNDIS
USB RNDIS network up!
Using usb_ether device
TFTP from server 192.168.100.1; our IP address is 192.168.100.2
Filename 'uImage'.
Load address: 0x81000000
Loading: T #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
######################################################
1.4 MiB/s
done
Bytes transferred = 12228888 (ba9918 hex)
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Linux-3.2.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 12228824 Bytes = 11.7 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.2.0 (matthew@matthew-ubuntu) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #2 Fri Apr 10 11:53:58 EDT 2015
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES2.1 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
[ 0.000000] Kernel command line: root=/dev/mmcblk0p2 rootwait console=ttyO0,115200
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 512MB = 512MB total
[ 0.000000] Memory: 499160k/499160k available, 25128k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc04ee000 (5016 kB)
[ 0.000000] .init : 0xc04ee000 - 0xc138d000 (14972 kB)
[ 0.000000] .data : 0xc138e000 - 0xc13ed0a8 ( 381 kB)
[ 0.000000] .bss : 0xc13ed0cc - 0xc141b344 ( 185 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000091] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[ 0.088836] pid_max: default: 32768 minimum: 301
[ 0.088928] Security Framework initialized
[ 0.089019] Mount-cache hash table entries: 512
[ 0.089324] CPU: Testing write buffer coherency: ok
[ 0.108612] omap_hwmod: pruss: failed to hardreset
[ 0.109527] print_constraints: dummy:
[ 0.109802] NET: Registered protocol family 16
[ 0.111450] OMAP GPIO hardware version 0.1
[ 0.113403] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.114868] omap_i2c.1: alias fck already exists
[ 0.115539] omap2_mcspi.1: alias fck already exists
[ 0.115692] omap2_mcspi.2: alias fck already exists
[ 0.116394] edma.0: alias fck already exists
[ 0.116394] edma.0: alias fck already exists
[ 0.116424] edma.0: alias fck already exists
[ 0.131195] bio: create slab <bio-0> at 0
[ 0.132812] SCSI subsystem initialized
[ 0.134063] usbcore: registered new interface driver usbfs
[ 0.134277] usbcore: registered new interface driver hub
[ 0.134429] usbcore: registered new device driver usb
[ 0.134674] registerd cppi-dma Intr @ IRQ 17
[ 0.134704] Cppi41 Init Done Qmgr-base(e087a000) dma-base(e0878000)
[ 0.134704] Cppi41 Init Done
[ 0.134704] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[ 0.134948] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[ 0.135772] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[ 0.136840] tps65910 1-002d: could not be detected
[ 0.138549] Switching to clocksource gp timer
[ 0.150054] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.150207] musb-hdrc musb-hdrc.0: dma type: dma-cppi41
[ 0.150451] MUSB0 controller's USBSS revision = 4ea20800
[ 0.150482] musb0: Enabled SW babble control
[ 0.151214] musb-hdrc musb-hdrc.0: USB OTG mode controller at e083c000 using DMA, IRQ 18
[ 0.151336] musb-hdrc musb-hdrc.1: dma type: dma-cppi41
[ 0.151580] MUSB1 controller's USBSS revision = 4ea20800
[ 0.151580] musb1: Enabled SW babble control
[ 0.151916] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.151977] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[ 0.152099] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.152099] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.152099] usb usb1: Product: MUSB HDRC host driver
[ 0.152130] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd
[ 0.152130] usb usb1: SerialNumber: musb-hdrc.1
[ 0.152770] hub 1-0:1.0: USB hub found
[ 0.152801] hub 1-0:1.0: 1 port detected
[ 0.153228] musb-hdrc musb-hdrc.1: USB Host mode controller at e083e800 using DMA, IRQ 19
[ 0.153564] NET: Registered protocol family 2
[ 0.153717] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.153961] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
[ 0.154174] TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.154296] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.154296] TCP reno registered
[ 0.154327] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.154327] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.154479] NET: Registered protocol family 1
[ 0.154663] RPC: Registered named UNIX socket transport module.
[ 0.154693] RPC: Registered udp transport module.
[ 0.154693] RPC: Registered tcp transport module.
[ 0.154693] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.238922] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.255798] VFS: Disk quotas dquot_6.5.2
[ 0.255859] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.256317] msgmni has been set to 974
[ 0.258758] alg: No test for stdrng (krng)
[ 0.259307] io scheduler noop registered
[ 0.259338] io scheduler deadline registered
[ 0.259399] io scheduler cfq registered (default)
[ 0.260345] Could not set LED4 to fully on
[ 0.299499] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 0.871337] console [ttyO0] enabled
[ 0.875366] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 0.883087] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 0.890777] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 0.898437] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 0.906127] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 0.914184] omap4_rng omap4_rng: OMAP4 Random Number Generator ver. 2.00
[ 0.928070] brd: module loaded
[ 0.935028] loop: module loaded
[ 0.938446] i2c-core: driver [tsl2550] using legacy suspend method
[ 0.944946] i2c-core: driver [tsl2550] using legacy resume method
[ 0.951385] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.049224] No daughter card found
[ 1.052795] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.067993] Board name: A335BNLT
[ 1.071380] Board version: 000C
[ 1.074645] The board is a AM335x Beaglebone Black.
[ 1.081817] tps65217 1-0024: TPS65217 ID 0xe version 1.2
[ 1.089355] print_constraints: DCDC1: 900 <--> 1800 mV at 1500 mV
[ 1.097747] print_constraints: DCDC2: 900 <--> 3300 mV at 1325 mV
[ 1.106140] print_constraints: DCDC3: 900 <--> 1500 mV at 1125 mV
[ 1.114532] print_constraints: LDO1: 1000 <--> 3300 mV at 1800 mV
[ 1.122924] print_constraints: LDO2: 900 <--> 3300 mV at 3300 mV
[ 1.131195] print_constraints: LDO3: 1800 <--> 3300 mV at 1800 mV
[ 1.139587] print_constraints: LDO4: 1800 <--> 3300 mV at 3300 mV
[ 1.146545] Maximum current provided by the USB port is 500mA which is not sufficient
[ 1.146545] when operating @OPP120 and OPPTURBO. The current requirement for some
[ 1.146545] use-cases using OPP100 might also exceed the maximum current that the
[ 1.146575] USB port can provide. Unless you are fully confident that the current
[ 1.146575] requirements for OPP100 use-case don't exceed the USB limits, switching
[ 1.146575] to AC power is recommended.
[ 1.190551] omap_hsmmc.0: alias fck already exists
[ 1.195953] omap_hsmmc.1: alias fck already exists
[ 1.201324] omap_i2c.3: alias fck already exists
[ 1.206512] omap_i2c omap_i2c.3: bus 3 rev2.4.0 at 100 kHz
[ 1.213989] registered am33xx_sr device
[ 1.219543] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.226562] omap2-nand driver initializing
[ 1.231018] OneNAND driver initializing
[ 1.235961] CAN device driver interface
[ 1.240020] CAN bus driver for Bosch D_CAN controller 1.0
[ 1.245941] usbcore: registered new interface driver cdc_ether
[ 1.252166] usbcore: registered new interface driver cdc_eem
[ 1.258178] usbcore: registered new interface driver dm9601
[ 1.264038] cdc_ncm: 04-Aug-2011
[ 1.267547] usbcore: registered new interface driver cdc_ncm
[ 1.273468] Initializing USB Mass Storage driver...
[ 1.278747] usbcore: registered new interface driver usb-storage
[ 1.285034] USB Mass Storage support registered.
[ 1.289916] gadget: using random self ethernet address
[ 1.295379] gadget: using random host ethernet address
[ 1.301330] usb0: MAC f6:78:5c:fc:60:b4
[ 1.305328] usb0: HOST MAC 4a:0f:cd:66:2c:b2
[ 1.309875] gadget: Ethernet Gadget, version: Memorial Day 2008
[ 1.316162] gadget: g_ether ready
[ 1.319732] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 1.325347] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2
[ 1.333190] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 1.340301] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 1.347839] usb usb2: Product: MUSB HDRC host driver
[ 1.353027] usb usb2: Manufacturer: Linux 3.2.0 musb-hcd
[ 1.358581] usb usb2: SerialNumber: musb-hdrc.0
[ 1.363983] hub 2-0:1.0: USB hub found
[ 1.367919] hub 2-0:1.0: 1 port detected
[ 1.372863] mousedev: PS/2 mouse device common for all mice
[ 1.379638] omap_rtc am33xx-rtc: rtc core: registered am33xx-rtc as rtc0
[ 1.386657] am33xx-rtc: already running
[ 1.390869] i2c /dev entries driver
[ 1.670013] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.677581] cpuidle: using governor ladder
[ 1.681884] gadget: high-speed config #2: RNDIS
[ 1.687225] cpuidle: using governor menu
[ 1.694793] omap4_aes_mod_init: loading AM33X AES driver
[ 1.700469] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02
[ 1.706878] omap4_aes_probe: probe() done
[ 1.711486] omap4_sham_mod_init: loading AM33X SHA/MD5 driver
[ 1.717681] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03
[ 1.747558] omap4_sham_probe: probe() done
[ 1.752502] oprofile: hardware counters not available
[ 1.757812] oprofile: using timer interrupt.
[ 1.762359] nf_conntrack version 0.5.0 (7799 buckets, 31196 max)
[ 1.769104] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 1.774810] TCP cubic registered
[ 1.778198] NET: Registered protocol family 17
[ 1.782897] can: controller area network core (rev 20090105 abi 8)
[ 1.789459] NET: Registered protocol family 29
[ 1.794097] can: raw protocol (rev 20090105)
[ 1.798583] can: broadcast manager protocol (rev 20090105 t)
[ 1.804534] Registering the dns_resolver key type
[ 1.809539] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 1.817596] ThumbEE CPU extension supported.
[ 1.822143] mux: Failed to setup hwmod io irq -22
[ 1.827636] Power Management for AM33XX family
[ 1.832519] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[ 1.839263] Copied the M3 firmware to UMEM
[ 1.843627] Cortex M3 Firmware Version = 0x181
[ 1.849121] create_regulator: DCDC2: Failed to create debugfs directory
[ 1.856719] smartreflex smartreflex: am33xx_sr_probe: Driver initialized
[ 1.867797] clock: disabling unused clocks to save power
[ 1.880035] mmc1: new high speed MMC card at address 0001
[ 1.888702] mmcblk0: mmc1:0001 MMC04G 3.60 GiB
[ 1.893829] mmcblk0boot0: mmc1:0001 MMC04G partition 1 2.00 MiB
[ 1.903472] mmcblk0boot1: mmc1:0001 MMC04G partition 2 2.00 MiB
[ 1.914276] mmcblk0: unknown partition table
[ 1.924163] mmcblk0boot1: unknown partition table
[ 1.934143] mmcblk0boot0: unknown partition table
[ 2.228240] omap_rtc am33xx-rtc: setting system clock to 2014-02-17 19:23:33 UTC (1392665013)
[ 2.255279] Freeing init memory: 14972K
INIT: version 2.88 booting
Starting udev
[ 4.197204] EXT3-fs (mmcblk0): error: can't find ext3 filesystem on dev mmcblk0.
[ 4.205596] EXT2-fs (mmcblk0): error: can't find an ext2 filesystem on dev mmcblk0.
[ 4.214111] FAT-fs (mmcblk0): bogus number of reserved sectors
[ 4.220214] FAT-fs (mmcblk0): Can't find a valid FAT filesystem
[ 4.240173] cramfs: wrong magic
[ 4.244049] FAT-fs (mmcblk0): bogus number of reserved sectors
[ 4.250183] FAT-fs (mmcblk0): Can't find a valid FAT filesystem
[ 4.523223] EXT3-fs (mmcblk0boot1): error: can't find ext3 filesystem on dev mmcblk0boot1.
[ 4.533782] EXT2-fs (mmcblk0boot1): error: can't find an ext2 filesystem on dev mmcblk0boot1.
[ 4.543823] FAT-fs (mmcblk0boot1): invalid media value (0x63)
[ 4.549896] FAT-fs (mmcblk0boot1): Can't find a valid FAT filesystem
[ 4.570007] EXT3-fs (mmcblk0boot0): error: can't find ext3 filesystem on dev mmcblk0boot0.
[ 4.584381] EXT2-fs (mmcblk0boot0): error: can't find an ext2 filesystem on dev mmcblk0boot0.
[ 4.594329] FAT-fs (mmcblk0boot0): bogus number of reserved sectors
[ 4.600921] FAT-fs (mmcblk0boot0): Can't find a valid FAT filesystem
[ 4.613067] cramfs: wrong magic
[ 4.620727] FAT-fs (mmcblk0boot1): invalid media value (0x63)
[ 4.626770] FAT-fs (mmcblk0boot1): Can't find a valid FAT filesystem
[ 4.640991] cramfs: wrong magic
[ 4.647369] FAT-fs (mmcblk0boot0): bogus number of reserved sectors
[ 4.654022] FAT-fs (mmcblk0boot0): Can't find a valid FAT filesystem
Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory
bootlogd.
Configuring network interfaces... ifconfig: SIOCGIFFLAGS: No such device
done.
Collected errors:
INIT: Entering runlevel: 5ot create lock file /var/lib/opkg/lock: No such fil
Starting syslogd/klogd: done
****************************************************
****************************************************
Sitara Flash Fetcher Script - 07/28/2014
udhcpc (v1.20.2) started
Sending discover...
Sending discover...
Sending discover...
Sending select for 192.168.100.22...
Lease of 192.168.100.22 obtained, lease time 600
Getting flasher script from server: 192.168.100.1
********************************************
Sitara Flash Fetcher is complete. Executing debrick.sh.
Calling Script=debrick.sh with SERVER_IP=192.168.100.1
****************************************************
****************************************************
Sitara Example Flashing Script - 02/11/2014
Getting files from server: 192.168.100.1
1+0 records in
1+0 records out
BusyBox v1.20.2 (2014-02-17 12:53:20 CST) multi-call binary.
Usage: tftp [OPTIONS] HOST [PORT]
Command exited with non-zero status 1
real 0m 0.03s
user 0m 0.00s
sys 0m 0.00s
No partition found. Continuing.
Partitioning the eMMC...
Checking that no-one is using th[ 12.145385] mmcblk0: unknown partition table
is disk right now ...
OK
[ 12.157867] mmcblk0: p1 p2rs, 255 heads, 63 sectors/track
sfdisk: ERROR: sector 0 does not have an msdos signature
sfdisk: /dev/mmcblk0: unrecognized partition table type
Old situation:
sfdisk: No partitions found
New situation:
Units = cylinders of 8225280 bytes, blocks of 1024 bytes, counting from 0
Device Boot Start End #cyls #blocks Id System
/dev/mmcblk0p1 * 0+ 8 9- 72261 c W95 FAT32 (LBA)
/dev/mmcblk0p2 10 469 460 3694950 83 Linux
/dev/mmcblk0p3 0 - 0 0 0 Empty
/dev/mmcblk0p4 0 - 0 0 0 Empty
Successfully wrote the new partition table
Re-reading the partition table ...
If you created or changed a DOS partition, /dev/foo7, say, then use dd(1)
to zero the first 512 bytes: dd if=/dev/zero of=/dev/foo7 bs=512 count=1
(See fdisk(8).)
[ 13.124206] EXT3-fs (mmcblk0p1): error: can't find ext3 filesystem on dev mmcblk0p1.
[ 13.134887] EXT3-fs (mmcblk0p2): error: can't find ext3 filesystem on dev mmcblk0p2.
[ 13.144927] EXT2-fs (mmcblk0p1): error: can't find an ext2 filesystem on dev mmcblk0p1.
[ 13.155273] EXT2-fs (mmcblk0p2): error: can't find an ext2 filesystem on dev mmcblk0p2.
[ 13.166168] FAT-fs (mmcblk0p1): bogus number of reserved sectors
[ 13.172546] FAT-fs (mmcblk0p1): Can't find a valid FAT filesystem
[ 13.182067] FAT-fs (mmcblk0p2): bogus number of reserved sectors
[ 13.188476] FAT-fs (mmcblk0p2): Can't find a valid FAT filesystem
real 0m 1.38s
user 0m 0.01s
sys 0m 0.27s
[ 13.287139] cramfs: wrong magic
[ 13.294219] FAT-fs (mmcblk0p1): bogus number of reserved sectors
[ 13.300628] FAT-fs (mmcblk0p1): Can't find a valid FAT filesystem
[ 13.317962] cramfs: wrong magic
[ 13.325073] FAT-fs (mmcblk0p2): bogus number of reserved sectors
[ 13.331420] FAT-fs (mmcblk0p2): Can't find a valid FAT filesystem
No partition found. Continuing.
1+0 records in
1+0 records out
Formatting the eMMC into 2 partitions...
mkfs.vfat 2.11 (12 Mar 2005)
mke2fs 1.42.1 (17-Feb-2012)
Discarding device blocks: done
Filesystem label=rootfs
OS type: Linux
Block size=4096 (log=2)
Fragment size=4096 (log=2)
Stride=0 blocks, Stripe width=0 blocks
231072 inodes, 923737 blocks
46186 blocks (5.00%) reserved for the super user
First data block=0
Maximum filesystem blocks=947912704
29 block groups
32768 blocks per group, 32768 fragments per group
7968 inodes per group
Superblock backups stored on blocks:
32768, 98304, 163840, 229376, 294912, 819200, 884736
Allocating group tables: done
Writing inode tables: done
Creating journal (16384 blocks): done
Writing superblocks and filesystem accounting information: done
Formatting done.
[ 30.076599] kjournald starting. Commit interval 5 seconds
[ 30.085540] EXT3-fs (mmcblk0p2): using internal journal
[ 30.091094] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
Copying Files...
real 0m 1.08s
user 0m 0.46s
sys 0m 0.40s
Boot partition done.
tar: no gzip/bzip2 magic
Command exited with non-zero status 1
real 0m 0.00s
user 0m 0.00s
sys 0m 0.00s
tar: can't open '-C': No such file or directory
Command exited with non-zero status 1
real 0m 0.00s
user 0m 0.00s
sys 0m 0.00s
RootFS partition done.
It took 20 seconds to complete this task...
********************************************
Sitara Example Flash Script is complete.
Stopping Bootlog daemon: bootlogd.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am335x-evm ttyO0
Arago 2013.05 am335x-evm ttyO0
am335x-evm login: [ 78.645782] tftp invoked oom-killer: gfp_mask=0x200d2, order=0, oom_adj=0, oom_score_adj=0
[ 78.654510] Backtrace:
[ 78.657104] [<c0017dbc>] (dump_backtrace+0x0/0x10c) from [<c039e638>] (dump_stack+0x18/0x1c)
[ 78.665924] r6:000200d2 r5:00000000 r4:ddd09280 r3:c13b13e8
[ 78.671875] [<c039e620>] (dump_stack+0x0/0x1c) from [<c007d29c>] (dump_header.isra.14+0x54/0x150)
[ 78.681182] [<c007d248>] (dump_header.isra.14+0x0/0x150) from [<c007d5ac>] (oom_kill_process.constprop.19+0x70/0x22c)
[ 78.692291] r8:ddea1cc0 r7:00000001 r6:000200d2 r5:00000000 r4:ddea1cc0
[ 78.699310] [<c007d53c>] (oom_kill_process.constprop.19+0x0/0x22c) from [<c007daf4>] (out_of_memory+0x23c/0x2d0)
[ 78.709960] [<c007d8b8>] (out_of_memory+0x0/0x2d0) from [<c00809c4>] (__alloc_pages_nodemask+0x640/0x664)
[ 78.719970] [<c0080384>] (__alloc_pages_nodemask+0x0/0x664) from [<c007b0c4>] (grab_cache_page_write_begin+0x54/0xc0)
[ 78.731079] [<c007b070>] (grab_cache_page_write_begin+0x0/0xc0) from [<c00c4b94>] (simple_write_begin+0x28/0x108)
[ 78.741821] [<c00c4b6c>] (simple_write_begin+0x0/0x108) from [<c0079f8c>] (generic_file_buffered_write+0x1a8/0x26c)
[ 78.752746] [<c0079de4>] (generic_file_buffered_write+0x0/0x26c) from [<c007ba98>] (__generic_file_aio_write+0x244/0x478)
[ 78.764221] [<c007b854>] (__generic_file_aio_write+0x0/0x478) from [<c007bd30>] (generic_file_aio_write+0x64/0xd0)
[ 78.775054] [<c007bccc>] (generic_file_aio_write+0x0/0xd0) from [<c00a602c>] (do_sync_write+0xac/0xec)
[ 78.784820] [<c00a5f80>] (do_sync_write+0x0/0xec) from [<c00a67a8>] (vfs_write+0xa4/0x148)
[ 78.793457] [<c00a6704>] (vfs_write+0x0/0x148) from [<c00a6a48>] (sys_write+0x40/0x78)
[ 78.801727] r8:00001000 r7:0009702c r6:c0820140 r5:00000000 r4:1da33000
[ 78.808776] [<c00a6a08>] (sys_write+0x0/0x78) from [<c0014740>] (ret_fast_syscall+0x0/0x30)
[ 78.817504] r8:c00148e8 r7:00000004 r6:00000004 r5:0009702c r4:00001000
[ 78.824554] Mem-info:
[ 78.826904] Normal per-cpu:
[ 78.829833] CPU 0: hi: 186, btch: 31 usd: 138
[ 78.834838] active_anon:324 inactive_anon:36 isolated_anon:0
[ 78.834838] active_file:897 inactive_file:0 isolated_file:0
[ 78.834838] unevictable:124715 dirty:0 writeback:0 unstable:0
[ 78.834869] free:702 slab_reclaimable:581 slab_unreclaimable:719
[ 78.834869] mapped:202 shmem:49 pagetables:43 bounce:0
[ 78.864593] Normal free:2808kB min:2884kB low:3604kB high:4324kB active_anon:1296kB inactive_anon:144kB active_file:3588kB inactive_file:0kB unevictable:498860kB isolated(anon):0kB isolated(file):0kB present:520192kB mlocked:0kB dirty:0kB writeback:0kB mapped:808kB shmem:196kB slab_reclaimable:2324kB slab_unreclaimable:2876kB kernel_stack:368kB pagetables:172kB unstable:0kB bounce:0kB writeback_tmp:0kB pages_scanned:124715 all_unreclaimable? yes
[ 78.905853] lowmem_reserve[]: 0 0
[ 78.909332] Normal: 0*4kB 1*8kB 1*16kB 1*32kB 1*64kB 1*128kB 0*256kB 1*512kB 0*1024kB 1*2048kB 0*4096kB 0*8192kB = 2808kB
[ 78.920837] 125661 total pagecache pages
[ 78.924926] 0 pages in swap cache
[ 78.928405] Swap cache stats: add 0, delete 0, find 0/0
[ 78.933868] Free swap = 0kB
[ 78.936859] Total swap = 0kB
[ 78.957305] 131072 pages of RAM
[ 78.960632] 936 free pages
[ 78.963470] 2539 reserved pages
[ 78.966766] 1300 slab pages
[ 78.969665] 1193 pages shared
[ 78.972778] 0 pages swap cached
[ 78.976074] [ pid ] uid tgid total_vm rss cpu oom_adj oom_score_adj name
[ 78.983886] [ 763] 0 763 444 178 0 -17 -1000 udevd
[ 78.991729] [ 941] 0 941 470 196 0 -17 -1000 udevd
[ 78.999572] [ 955] 0 955 443 190 0 -17 -1000 udevd
[ 79.007446] [ 1277] 0 1277 457 139 0 0 0 syslogd
[ 79.015472] [ 1280] 0 1280 457 133 0 0 0 klogd
[ 79.023345] [ 1297] 0 1297 457 58 0 0 0 udhcpc
[ 79.031311] [ 1304] 0 1304 424 98 0 0 0 time
[ 79.039062] [ 1309] 0 1309 457 130 0 0 0 tftp
[ 79.046813] [ 1422] 0 1422 393 124 0 0 0 getty
[ 79.054687] [ 1423] 0 1423 393 124 0 0 0 getty
[ 79.062561] Out of memory: Kill process 1277 (syslogd) score 1 or sacrifice child
[ 79.070404] Killed process 1277 (syslogd) total-vm:1828kB, anon-rss:60kB, file-rss:496kB
[ 79.176849] tftp invoked oom-killer: gfp_mask=0x200d2, order=0, oom_adj=0, oom_score_adj=0
[ 79.185546] Backtrace:
[ 79.188140] [<c0017dbc>] (dump_backtrace+0x0/0x10c) from [<c039e638>] (dump_stack+0x18/0x1c)
[ 79.196960] r6:000200d2 r5:00000000 r4:ddd09280 r3:c13b13e8
[ 79.202911] [<c039e620>] (dump_stack+0x0/0x1c) from [<c007d29c>] (dump_header.isra.14+0x54/0x150)
[ 79.212188] [<c007d248>] (dump_header.isra.14+0x0/0x150) from [<c007d5ac>] (oom_kill_process.constprop.19+0x70/0x22c)
[ 79.223297] r8:c0843980 r7:00000001 r6:000200d2 r5:00000000 r4:c0843980
[ 79.230316] [<c007d53c>] (oom_kill_process.constprop.19+0x0/0x22c) from [<c007daf4>] (out_of_memory+0x23c/0x2d0)
[ 79.240997] [<c007d8b8>] (out_of_memory+0x0/0x2d0) from [<c00809c4>] (__alloc_pages_nodemask+0x640/0x664)
[ 79.251007] [<c0080384>] (__alloc_pages_nodemask+0x0/0x664) from [<c007b0c4>] (grab_cache_page_write_begin+0x54/0xc0)
[ 79.262207] [<c007b070>] (grab_cache_page_write_begin+0x0/0xc0) from [<c00c4b94>] (simple_write_begin+0x28/0x108)
[ 79.272949] [<c00c4b6c>] (simple_write_begin+0x0/0x108) from [<c0079f8c>] (generic_file_buffered_write+0x1a8/0x26c)
[ 79.283874] [<c0079de4>] (generic_file_buffered_write+0x0/0x26c) from [<c007ba98>] (__generic_file_aio_write+0x244/0x478)
[ 79.295349] [<c007b854>] (__generic_file_aio_write+0x0/0x478) from [<c007bd30>] (generic_file_aio_write+0x64/0xd0)
[ 79.306182] [<c007bccc>] (generic_file_aio_write+0x0/0xd0) from [<c00a602c>] (do_sync_write+0xac/0xec)
[ 79.315917] [<c00a5f80>] (do_sync_write+0x0/0xec) from [<c00a67a8>] (vfs_write+0xa4/0x148)
[ 79.324584] [<c00a6704>] (vfs_write+0x0/0x148) from [<c00a6a48>] (sys_write+0x40/0x78)
[ 79.332855] r8:00001000 r7:0009702c r6:c0820140 r5:00000000 r4:1dad0000
[ 79.339904] [<c00a6a08>] (sys_write+0x0/0x78) from [<c0014740>] (ret_fast_syscall+0x0/0x30)
[ 79.348632] r8:c00148e8 r7:00000004 r6:00000004 r5:0009702c r4:00001000
[ 79.355651] Mem-info:
[ 79.358032] Normal per-cpu:
[ 79.360961] CPU 0: hi: 186, btch: 31 usd: 113
[ 79.366027] active_anon:309 inactive_anon:36 isolated_anon:0
[ 79.366027] active_file:0 inactive_file:0 isolated_file:0
[ 79.366027] unevictable:125769 dirty:0 writeback:0 unstable:0
[ 79.366027] free:708 slab_reclaimable:468 slab_unreclaimable:719
[ 79.366027] mapped:196 shmem:49 pagetables:39 bounce:0
[ 79.395599] Normal free:2832kB min:2884kB low:3604kB high:4324kB active_anon:1236kB inactive_anon:144kB active_file:0kB inactive_file:0kB unevictable:503076kB isolated(anon):0kB isolated(file):0kB present:520192kB mlocked:0kB dirty:0kB writeback:0kB mapped:784kB shmem:196kB slab_reclaimable:1872kB slab_unreclaimable:2876kB kernel_stack:360kB pagetables:156kB unstable:0kB bounce:0kB writeback_tmp:0kB pages_scanned:1054 all_unreclaimable? yes
[ 79.436431] lowmem_reserve[]: 0 0
[ 79.439910] Normal: 58*4kB 1*8kB 0*16kB 1*32kB 0*64kB 2*128kB 1*256kB 2*512kB 1*1024kB 0*2048kB 0*4096kB 0*8192kB = 2832kB
[ 79.451507] 125818 total pagecache pages
[ 79.455627] 0 pages in swap cache
[ 79.459106] Swap cache stats: add 0, delete 0, find 0/0
[ 79.464569] Free swap = 0kB
[ 79.467559] Total swap = 0kB
[ 79.487884] 131072 pages of RAM
[ 79.491210] 913 free pages
[ 79.494018] 2539 reserved pages
[ 79.497314] 1187 slab pages
[ 79.500213] 1070 pages shared
[ 79.503326] 0 pages swap cached
[ 79.506591] [ pid ] uid tgid total_vm rss cpu oom_adj oom_score_adj name
[ 79.514373] [ 763] 0 763 444 178 0 -17 -1000 udevd
[ 79.522186] [ 941] 0 941
到這邊就停住了....
[Uniflash 狀態]
[debrick.sh]
echo "****************************************************"
echo "****************************************************"
echo ""
echo "Sitara Example Flashing Script - 02/11/2014"
echo ""
STARTTIME=$(date +%s)
##---------Start of variables---------------------##
## Set Server IP here
SERVER_IP="192.168.100.1"
## Names of the images to grab from TFTP server
BOOT_PARTITION="boot_partition.tar.gz"
## Rename rootfs as needed depending on use of tar or img
ROOTFS_PARTITION="rootfs_partition.tar.gz"
##ROOTFS_USR="usr.tar.gz"
## ROOTFS_PARTITION="rootfs_partition/"
## ROOTFS_PARTITION="rootfs_partition.img.gz"
## Declare eMMC device name here
DRIVE="/dev/mmcblk0"
##----------End of variables-----------------------##
## TFTP files from host. Edit the files and host IP address for your application.
## We are grabbing two files, one an archive with files to populate a FAT partion,
## which we will create. Another for a filesystem image to 'dd' onto an unmounted partition.
## Using a compressed tarball can be easier to implement, however, with a large file system
## with a lot of small files, we recommend a 'dd' image of the partition to speed up writes.
echo "Getting files from server: ${SERVER_IP}"
time tftp -b 4096 -g -r ${BOOT_PARTITION} ${SERVER_IP} &
boot_pid=$!
time tftp -b 4096 -g -r ${ROOTFS_PARTITION} ${SERVER_IP} &
rootfs_pid=$!
time tftp -b 4096 -g -r ${ROOTFS_USR} ${SERVER_IP} &
rootfs_pid=$!
## Kill any partition info that might be there
dd if=/dev/zero of=$DRIVE bs=4k count=1
sync
sync
## Figure out how big the eMMC is in bytes
SIZE=`fdisk -l $DRIVE | grep Disk | awk '{print $5}'`
## Translate size into segments, which traditional tools call Cylinders. eMMC is not a spinning disk.
## We are basically ignoring what FDISK and SFDISK are reporting because it is not really accurate.
## we are translating this info to something that makes more sense for eMMC.
CYLINDERS=`echo $SIZE/255/63/512 | bc`
## Check to see if the eMMC partitions have automatically loaded from the old MBR.
## This might have occured during the boot process if the kernel detected a filesystem
## before we killed the MBR. We will need to unmount and kill them by writing 4k zeros to the
## partitions that were found.
check_mounted(){
is_mounted=$(grep ${DRIVE}p /proc/mounts | awk '{print $2}')
if grep -q ${DRIVE}p /proc/mounts; then
echo "Found mounted partition(s) on " ${DRIVE}": " $is_mounted
umount $is_mounted
counter=1
for i in $is_mounted; do \
echo "4k erase on ${DRIVE}p${counter}";
dd if=/dev/zero of=${DRIVE}p${counter} bs=4k count=1;
counter=$((counter+1));
done
else
echo "No partition found. Continuing."
fi
}
check_mounted;
## Partitioning the eMMC using information gathered.
## Here is where you can add/remove partitions.
## We are building 2 partitions:
## 1. FAT, size = 9 cylinders * 255 heads * 63 sectors * 512 bytes/sec = ~70MB
## 2. EXT3, size = 223 ($CYLINDERS-[9 for fat]) cylinders * 255 heads * 63 sectors * 512 bytes/sec = ~1l.7GB
##
## You will need to change the lines ",9,0c0C,*", "10,,,-" to suit your needs. Adding is similar,
## but you will need to be aware of partition sizes and boundaries. Use the man page for sfdisk.
echo "Partitioning the eMMC..."
sfdisk -D -H 255 -S 63 -C $CYLINDERS $DRIVE << EOF
,9,0x0C,*
10,,,-
EOF
## This sleep is necessary as there is a service which attempts
## to automount any filesystems that it finds as soon as sfdisk
## finishes partitioning. We sleep to let it run. May need to
## be lengthened if you have more partitions.
sleep 2
## Check here if there has been a partition that automounted.
## This will eliminate the old partition that gets
## automatically found after the sfdisk command. It ONLY
## gets found if there was a previous file system on the same
## partition boundary. Happens when running this script more than once.
## To fix, we just unmount and write some zeros to it.
check_mounted;
## Clean up the dos (FAT) partition as recommended by SFDISK
dd if=/dev/zero of=${DRIVE}p1 bs=512 count=1
## Make sure posted writes are cleaned up
sync
sync
## Format the eMMC into 2 partitions
echo "Formatting the eMMC into 2 partitions..."
## Format the boot partition to fat32
mkfs.vfat -F 32 -n "boot" ${DRIVE}p1
## Format the rootfs to ext3 (or ext4, etc.) if using a tar file.
## We DO NOT need to format this partition if we are 'dd'ing an image
## Comment out this line if using 'dd' of an image.
mkfs.ext3 -L "rootfs" ${DRIVE}p2
## Make sure posted writes are cleaned up
sync
sync
echo "Formatting done."
## Make temp directories for mountpoints
mkdir tmp_boot
## Comment this line out if using 'dd' of an image. It is not needed.
mkdir tmp_rootfs
## Mount partitions for tarball extraction. NOT for 'dd'.
mount -t vfat ${DRIVE}p1 tmp_boot
## If 'dd'ing the rootfs, there is no need to mount it. Comment out the below.
mount -t ext3 ${DRIVE}p2 tmp_rootfs
## Wait for boot to finish tftp
wait $boot_pid
echo "Copying Files..."
time tar -xf ${BOOT_PARTITION} -C tmp_boot
sync
sync
umount ${DRIVE}p1
rm ${BOOT_PARTITION}
echo "Boot partition done."
## Wait for rootfs to finish tftp
wait $rootfs_pid
## If using a tar archive, untar it with the below.
## If using 'dd' of an img, comment these lines out and use the below.
#time tar -zxvf ${ROOTFS_PARTITION} -C
time tar -xf ${ROOTFS_PARTITION} -C tmp_rootfs
#time cp -r ${ROOTFS_PARTITION} tmp_rootfs
sync
sync
time tar -xf ${ROOTFS_USR} -C tmp_rootfs
sync
sync
umount ${DRIVE}p2
rm ${ROOTFS_PARTITION}
echo "RootFS partition done."
## If using 'dd' of an img, uncomment these lines.
## If using a tar archive, comment out these lines and use the above.
## time gunzip -c ${ROOTFS_PARTITION} | dd of=${DRIVE}p2 bs=4k
## sync
## sync
## echo "Rootfs partition done."
## The block below is only necessary if using 'dd'.
## Force check the filesystem for consistency and fix errors if any.
## Resize partition to the length specified by the MBR.
## /sbin/e2fsck -fy ${DRIVE}p2
## /sbin/resize2fs ${DRIVE}p2
ENDTIME=$(date +%s)
echo "It took $(($ENDTIME - $STARTTIME)) seconds to complete this task..."
## Reboot
echo ""
echo "********************************************"
echo "Sitara Example Flash Script is complete."
echo ""
重新啟動後僅能進入UBOOT MODE :
U-Boot SPL 2015.07-00114-gf5078ef-dirty (Feb 23 2016 - 18:30:35)
reading args
spl_load_image_fat_os: error reading image args, err - -1
reading u-boot.img
reading u-boot.img
U-Boot 2015.07-00114-gf5078ef-dirty (Feb 23 2016 - 18:30:35 +0800)
Watchdog enabled
I2C: ready
DRAM: 512 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Card did not respond to voltage select!
** Bad device mmc 0 **
Using default environment
Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw, usb_ether
Hit any key to stop autoboot: 0
Card did not respond to voltage select!
Card did not respond to voltage select!
switch to partitions #0, OK
mmc1(part 0) is current device
SD/MMC found on device 1
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
** Unable to read file uEnv.txt **
** File not found /boot/zImage **
Booting from nand ...
no devices available
no devices available
Bad Linux ARM zImage magic!
U-Boot#
或是有相關建議的朋友可以給予建議與指導,非常感謝!!
周工 你好 :
我现在按照您提供的文档,用sdk6的代码可以usb烧录了,但我想移植到我自己的板子使用,用debrick.sh脚本将系统文件写入emmc后,烧录自己板子的uboot后卡在这里:
U-Boot SPL 2011.09 (Jun 18 2014 - 09:38:14)
ZHD-AM335x-Evaluation.
boot mode - RAW
mkimage signature not found - ih_magic = 0
Assuming u-boot.bin ..
我怀疑是不是烧写系统时偏移地址的问题,因为和我现在uboot的偏移地址不对应,因为uboot之前是别的同事移植的,我不熟悉这方面的烧写,我想问下:
sfdisk -D -H 255 -S 63 -C $CYLINDERS $DRIVE << EOF
7,9,0x0C,*
10,,,-
EOF
这一段是什么含义,怎么使用sfdisk命令,怎么设置分区时的初始地址,我的emmc大小是16G,网上找不到sfdisk具体操作、、
#define MLO_ADDR 0x20000
#define MLO_SIZE (1024*100)
#define UBOOT_ADDR 0x60000
#define UBOOT_SIZE (1024*256)
#define KERNEL_ADDR 0x100000
#define KERNEL_SIZE (1024*1024*2.5)
#define ROOTFS_ADDR 0x500000
#define ROOTFS_SIZE (1024*1024*2.8)
这个是我自己板子的uboot需要偏移的地址说明,按照这个我要怎么用sfdisk去调整参数分区,或者是还有没有其它方法命令可以去执行?
有点急 ,麻烦大家了!!谢谢!!
烧录的整个过程都是正确的么?你烧录的Linux应该不是TI的SDK吧?
jian zhou 你好 我使用的是sdk6.0版本的 按照您这个文档做的emmc烧写,现在遇见一个 问题,在uniflash下载软件中的 进度条进行到27%的时候就不能运行了
下面是我串口接收到的数据